STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 isochronous transfer

Posted on December 19, 2014 at 08:33 how to transfer 512 bytes? Send_DATA ((unsigned char *)trBuffer, 512); void Send_DATA(uint8_t* ptrBuffer, uint16_t Send_length) { if (GetENDPOINT(ENDP1) & EP_DTOG_RX) // NOT TX ie SW_BUF { U...

FatFS problem with SDIO on stm32f103vet6

Posted on December 18, 2014 at 16:23Hi guys, I'm trying to use an SD card with the aforementioned chip on the Primer2. I started from a working project but when ported to my application, it simply doesn't work. Anyone can help?In detail, I've ported...

angeletti by Associate II
  • 2855 Views
  • 8 replies
  • 0 kudos

STM32F072 temp sensor counts wrong way !!

Posted on December 18, 2014 at 21:25Hi I'm just playing around with the discovery board ST32F0so I wrote a quick and dirty C app in CoIDE, started a ADC conversion etc and read in the on chip temp sensor. Thats all works fine ( or so it seems) even ...

STM32F407 USART3 DMA Transmit problem

Posted on December 18, 2014 at 13:32 Hello Everyone I am tryint to send data through usart3 by dma ; I can send data without DMA but when configure to use the DMA I could not send ; Could you guide me to check my mistakes ; the code ...

DIfferent Vector tables or single one

Posted on December 18, 2014 at 11:57now I have 2 hex files running independently, to perform context switching i am using a systick timer, now should i use a single vector table to link them by calling same ISR, or define 2 Vector tables and call 2 ...

STM32F103ZET6, write protection

Posted on December 15, 2014 at 13:50Gentlem, my question: The STMFlashDemonstrator 2.7.0 after loading a program in to the STM32F103ZET6, while verifying, brings the error: ''...The page may be write protected. Please disable the write protection......

frantzw by Associate II
  • 1427 Views
  • 3 replies
  • 0 kudos

Mistake?

Posted on December 10, 2014 at 11:10The original post was too long to process during our migration. Please click on the attachment to read the original post.

franck2 by Associate II
  • 2408 Views
  • 5 replies
  • 0 kudos