STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fatfs Unicode

Posted on January 19, 2015 at 10:57Hi Guys,I previously had code working with Fatfs and I had LFN enabled but LFN_Unicode disabled. I now want to start using Unicode, but after enabling it in the ffconf.h file, my fat functions return FR_NOT_READY a...

STM32F407ZGT, SPI3 and Debugging with SWD

Posted on January 12, 2015 at 10:52Hello, i'm using an STM32F407ZET6 with SPI1, SPI2, SP3 and SWD. SPI1 and SPI2 are always working fine. SPI3 works when the CPU is running without debugging. Whenever I set a breakpoint SPI3 Clock (PortB3) has stran...

0690X00000604sHQAQ.png 0690X00000604KoQAI.png
mkunz9 by Associate II
  • 3925 Views
  • 7 replies
  • 0 kudos

Where is STM32CubeMX Software?

Posted on January 16, 2015 at 22:06I can't seem to find the download software link for the CubeMX software?  The link I have is here:http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?s_searchtype=partnumber This link only has do...

STM32F427: Trouble getting OCx to work with TIM8

Posted on January 19, 2015 at 21:22The complete project is https://my.st.com//public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/49654/TIM8_OC.zip.I've made a simple test-program, which toggles some LEDs.I'd like PC6-PC9 to toggle automat...

pacman by Associate III
  • 1030 Views
  • 2 replies
  • 0 kudos

STM32 FMC and nor flash

Posted on January 19, 2015 at 21:19I've been reading through this (rather complex) datasheet for NOR flash.http://www.micron.com/~/media/documents/products/data-sheet/nor-flash/parallel/m29w/m29w128g.pdfIt's the same flash that the STM32F439xI EVAL ...

Stm32f407 hang up in system memory when debug

Posted on January 19, 2015 at 20:00Hello everybody! I've a very strange error. I've running application for stm32f407. I can download the code and it's working well. But when I want to debug with CoIDE the code stopped at 1FFF39c4 so in the system m...

totti001 by Associate II
  • 680 Views
  • 0 replies
  • 0 kudos

DFU: LEAVE does not jump to application.

Posted on January 13, 2015 at 16:52 I want to jumper my STM32F072 processor for ''boot to system memory'': DFU mode. Then I want to use software to ''start the application''. This should be possible.AN3156 section 5.5 tells me that after a...

Issue while Enabling and Disabling Timer

Posted on January 19, 2015 at 06:54Basically what my problem is Once I de-init the Timer after a successful operation I'm not able to re-init it again...I am writing a program to generate a delay using timer whose delay canbe varied according to the...

How to run corect PID trough STM32F4 and matlab

Posted on January 19, 2015 at 06:32 Hello all, i am trying to do a simple pid simulation with discovery board and matlab. However i dont think that my data is runing as it should, what i want to say is that i dont get the usualy rising s...

0690X00000605EHQAY.png 0690X00000605EMQAY.png
Bogdan by Senior
  • 1304 Views
  • 0 replies
  • 0 kudos