STM32F207 SPI-Ethernet bridge maximum bit rate
Posted on January 23, 2015 at 15:43HiI'm using STM32F207.The task is to receive continuous stream of data on spi slave input at a speed of about 10-15 mbps. The data must be then buffered into the RAM and then transmitted as the packets over Etherne...