STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change Timer PWM Output Pulse On the Fly

Posted on January 28, 2015 at 21:29Hi, I have figured out how to change the period of the Timer 3 on the fly by using TIM3->CNT = someNewValue; and it works good. However, the duty cycle requires updating as well, set up originally as PWM pulse (TI...

SPI PIN Configuration for STM32F0

Posted on January 10, 2015 at 10:14Dear All,I would be grate if any one could advice me that in which page the SPI pin configuration is showing in the ''RM0091Reference manual'' STM32F0I mean, What are the proper  Configure GPIO for MOSI, MISO and S...

pic_micro by Associate II
  • 8084 Views
  • 24 replies
  • 0 kudos

ARM GNU Eclipse plugin and SPL

Posted on January 28, 2015 at 14:26Hello there, I am using eclipse and arm gnu eclipse plugin. It comes with HAL instead of SPL. Most of the available examples out there are SPL and I need to rely on that as I am a begginer in STM32 world. So i trie...

DMA tranfer from GPIO IDR to RAM

Posted on January 27, 2015 at 14:10I'm new to STM32 board. Working with F103C8, currently I could use TIM2 (24M) as trigger source to start DMA1 to transfer data from GPIOB->IDR(15:0) to RAM. However I found the speed is no more than 8MHz during the...

leonlawww by Associate II
  • 3751 Views
  • 7 replies
  • 0 kudos

STM32F429 Timer1 Capture/Compare with IRQ

Posted on January 28, 2015 at 13:02Hello, I use the Timer1 in capture compare mode. I want the following function: 1. Timer1 starts to count from 0 2. Timer1 counter register is the same, like in compare register     => IRQ_CC 3. Timer1 counter regi...

der-kyle by Associate II
  • 1469 Views
  • 2 replies
  • 0 kudos

PEGM2701

Posted on January 28, 2015 at 13:58Hi Is there a micro from ST with marking PEGM2701? Regards Hossam Alzomor

hossam by Associate II
  • 1039 Views
  • 1 replies
  • 0 kudos

Measuring the input signal frequncy with stm32f4

Posted on January 27, 2015 at 18:27Hello everyone, I am new to STM32f4 board. I would like to measure speed of a dc motor(in terms of input signal frequency which varies from 0 Hz to 50KHz). Actually I have only one signal (so I think I can't use en...

naren by Associate II
  • 2391 Views
  • 5 replies
  • 0 kudos

HAL documentation: .CHM files?

Posted on January 24, 2015 at 06:52The older ''Standard Peripheral Library'' came with a really wonderful .CHM file that cross-indexed all the documentation and source code. Is that available for the new ST Cube libraries (and the HAL in particular)...

westfw by Associate II
  • 2367 Views
  • 3 replies
  • 0 kudos

Cube HAL documentation

Posted on January 28, 2015 at 09:32Hello,Where can we find documentation for STM32F HAL API, generated by Cube?Thanks!

George.P by Associate III
  • 1254 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.