STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C8T6 SPI DMA wrong bytes position

Posted on January 27, 2015 at 10:25My STM32f103C8T6 works as a slave. The SPI DMA worked fine if I put the NSS pin of the slave to the ground or set the pins config to software. But if I put the NSS pin of the slave to the gpio pin of the master, th...

tn88test by Associate II
  • 1550 Views
  • 3 replies
  • 0 kudos

STM32_Mass_Storage_Readfile

Posted on January 29, 2015 at 08:10Dear All.I'm working with SMT32F103 USB function.STM32F103 board is mass storage device now.Now the PC recognize and can read/write file to internal flash memory of STM32F103.(Example: text file, bitmap file, jpeg ...

Error while programming my STM32F105 board using SWD

Posted on January 28, 2015 at 11:19Dear all,           I am using STM32F0 discovery board to program my STM32F105 board. I am getting below errors, can any body suggest15:37:20 : The elf loader Program function fails.15:37:21 : Memory-Loader error15...

maulin by Associate II
  • 1496 Views
  • 3 replies
  • 0 kudos

Change Timer PWM Output Pulse On the Fly

Posted on January 28, 2015 at 21:29Hi, I have figured out how to change the period of the Timer 3 on the fly by using TIM3->CNT = someNewValue; and it works good. However, the duty cycle requires updating as well, set up originally as PWM pulse (TI...

SPI PIN Configuration for STM32F0

Posted on January 10, 2015 at 10:14Dear All,I would be grate if any one could advice me that in which page the SPI pin configuration is showing in the ''RM0091Reference manual'' STM32F0I mean, What are the proper  Configure GPIO for MOSI, MISO and S...

pic_micro by Associate II
  • 7644 Views
  • 24 replies
  • 0 kudos

ARM GNU Eclipse plugin and SPL

Posted on January 28, 2015 at 14:26Hello there, I am using eclipse and arm gnu eclipse plugin. It comes with HAL instead of SPL. Most of the available examples out there are SPL and I need to rely on that as I am a begginer in STM32 world. So i trie...

DMA tranfer from GPIO IDR to RAM

Posted on January 27, 2015 at 14:10I'm new to STM32 board. Working with F103C8, currently I could use TIM2 (24M) as trigger source to start DMA1 to transfer data from GPIOB->IDR(15:0) to RAM. However I found the speed is no more than 8MHz during the...

leonlawww by Associate II
  • 3610 Views
  • 7 replies
  • 0 kudos

STM32F429 Timer1 Capture/Compare with IRQ

Posted on January 28, 2015 at 13:02Hello, I use the Timer1 in capture compare mode. I want the following function: 1. Timer1 starts to count from 0 2. Timer1 counter register is the same, like in compare register     => IRQ_CC 3. Timer1 counter regi...

der-kyle by Associate II
  • 1408 Views
  • 2 replies
  • 0 kudos

PEGM2701

Posted on January 28, 2015 at 13:58Hi Is there a micro from ST with marking PEGM2701? Regards Hossam Alzomor

hossam by Associate II
  • 993 Views
  • 1 replies
  • 0 kudos