STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C weird read value return in STM32F429I Disco

Posted on February 16, 2015 at 10:52Hey everyone,I am trying to get the Device ID of an I2C connected image sensor for our project but somehow the value keeps returning 0x00. I did recieve the Device ID (0xA0) a couple of times but could not do so o...

mitjaneho by Associate II
  • 1093 Views
  • 1 replies
  • 0 kudos

two STM32 micro USART communication

Posted on February 14, 2015 at 14:33In my design, I am using two STM32 micro communicate with USART, the connection is as below, these two micro is in same board, and the communicate trace line length is around 1.5 inch. STM32F030 (USART1_TX)  PA9--...

STM32F407 Half Duplex

Posted on February 13, 2015 at 11:33Hi,I am trying to figure what I need to set the SPI peripheral to communicate to a device which can be configured to be master or slave and has a single data bus.The slave device has the following pins - SCK, DATA...

paul23 by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos

STM32F101 is not responding to reset

Posted on February 14, 2015 at 07:42Hi,We have a trouble with STM32F101. We used STM32F101 for far field device. It passed all EMI/EMC test for CE, then we started to field installation.After a while, server communication was lost with some devices....

mustafa by Associate II
  • 3843 Views
  • 8 replies
  • 0 kudos

stm32f4 spi problem

Posted on February 14, 2015 at 14:57Hi, the code for my interrupt handler is belowvoid SPI_IRQHandler(SPI_TypeDef * SPIx){ uint8_t SPIn = (SPIx == SPI1) ? 0 : ((SPIx == SPI2) ? 1 : 2); if(SPI_I2S_GetITStatus(SPIx, SPI_I2S_IT_RXNE) == SET) { if(_RxCo...

dsp

Posted on February 07, 2015 at 18:46  The original post was too long to process during our migration. Please click on the attachment to read the original post.

kemal by Associate II
  • 1138 Views
  • 2 replies
  • 0 kudos

Meassuring frequency of external signal

Posted on February 14, 2015 at 12:39Hi, is it possible to meassure frequency of external signal via Input capture, if the external signal is only from 0,5V to 2,5V (not from 0V to Vdd - 3V) and it is sine wave (not square wave)?Thank you

jelinpe7 by Associate
  • 1199 Views
  • 2 replies
  • 0 kudos

CPAL I2C Issue

Posted on April 12, 2012 at 16:30One of my colleague has an issue with CPAL that ppl might have seen before (when being used for I2C communication on the SMT32L15R6...It appears to do start communicating, sends the start, sends the address and then ...

MikeAtETI by Associate III
  • 956 Views
  • 2 replies
  • 0 kudos

How to corretly stop timer

Posted on February 13, 2015 at 21:41Hello, I am measuring voltage via ADC, using timer TRGO interrupt trgiggered DMA. After measuring 1000samples I need to stop, proces meassured data and then continue in meassuring. I stop timer by:TIM_ITConfig(TIM...

j3lda by Associate II
  • 1293 Views
  • 2 replies
  • 0 kudos

Struggling with HC05 Module for AT Command

Posted on February 13, 2015 at 16:57I'm getting some hard time trying to make my HC05 to execute an AT command from my stm32f4 , first it seemed that the problem was that the module was not in AT mode, now that i got it to enter AT mode it still is ...

monta by Associate II
  • 2992 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.