STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM Input capture and PWM output with same timer

Posted on March 27, 2015 at 16:06Hi, I'm working with an STM32F103RB.I try to do a PWM input capture (frequency and duty) and also PWM     output with the same TIMER.It seems there is a problem.My pwm output restarts when a rising edge occurs on the...

eancelin by Associate II
  • 2094 Views
  • 1 replies
  • 0 kudos

LSE and HSE on MCO1

Posted on March 26, 2015 at 09:56 I use STM32F4 I set MCO1 to PLL Clock and set output prescaler to 5 and I have 6MHz on my MCO1. There is no problem in it, But when I enable LSE with HSE together, I have no signal on MCO1 pin. Code: ...

STM32F100C6 USART TX pin floating after stopbit

Posted on March 25, 2015 at 13:32Hi Issue:Using USART, configured as a normal uart full duplex, we see that the TX pin from the MCU is floating after the stopbit. This seems to be causing issues in some cases.Question 1:What is the default behavior ...

kimtommy by Associate II
  • 1951 Views
  • 3 replies
  • 0 kudos

32F429IDISCOVERY RAM extension

Posted on March 20, 2015 at 15:02Hi,I am having a problem with RAM shortage on 32F429IDISCOVERY because of a complex processing algorithm. Generally speaking heap crushes into my stack and hard fault is called. The algorithm that I use cannot be cha...

Can you trust Real-time clock powered by Supercapacitor

Posted on March 26, 2015 at 11:38Is there a way to tell if the reading in the real-time-clock is valid - i.e. that the clock has kept ticking since the last time it was set?My board has a STM32f405, and its backup domain is powered by a Supercapacit...

Danish1 by Lead III
  • 2538 Views
  • 3 replies
  • 0 kudos

STM32F429 Discovery kit pinout

Posted on April 29, 2014 at 15:01Hello, I have to develop a board to attach to an STM32F429 Discovery kit to control a comercial display. In the design i found that the pins of the discovery kit give only a certain funcionality. Is not other way of ...

alimed by Associate II
  • 3833 Views
  • 8 replies
  • 0 kudos

UM1724, wrong pin

Posted on March 27, 2015 at 11:43DocID025833 Rev 7, pg 25/63, description of SB62, SB63: Reads (twice):   ... to D1 and D0 (pin 7 and pin 8) on Arduino connector CN9 ... Should read:   ... to D1 and D0 (pin 2 and pin 1) on Arduino connector CN9 ...

Image Capture using STM32F2

Posted on March 27, 2015 at 05:21I have developed a stm32f207 board for my own application. I have interfaced a 14 bit grayscale camera using DCMI. I'm then transferring this image to the SRAM using DMA. The SRAM being used is the same present on th...

0690X00000602oSQAQ.jpg 0690X000006030rQAA.jpg

How to watch variables in CubeMX

Posted on March 23, 2015 at 08:53Hello. I'd like to know how to refer values of variables. My understanding is all of variables are seen in a variable scope when I stop a program, but at the moment, I can't look at some variables I defined. Could so...

STM32F411 I2S1 supply dma?

Posted on March 26, 2015 at 09:02Hi,I want use I2S function on ST411I2S1(SPI1) can work on DMA Mode?I check DMA1 request mapping Only have I2S2 , I2S3 but in my design need SDIO (SPI2,SPI3) #i2s-stm32f411

cyan1650 by Associate
  • 1177 Views
  • 2 replies
  • 0 kudos