STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 with EEPROM

Posted on March 31, 2015 at 17:19Why doesn't ST embed an EEPROM in STM32F4xx or STM32F1xx series?Thanks.

STM32 AHB multilayer bus arbiter

Posted on April 01, 2015 at 18:22Hi I read the AN4031 application note ''Using the STM32F2 and STM32F4 DMA controller''. In this document it is mentioning that the AHB Multi layer bus has an Arbiter on each layer, which handles the bus arbitration ...

Any hints of plans for STM32F7 based Nucleo boards?

Posted on March 25, 2015 at 18:37I can't seem to find any statements about plans for ST to deliver a Nucleo board with a STM32F7 chip.  I would appreciate any pointers or news you might have. Is it worth waiting for a bit, or is it time to experimen...

STM32L152RE NUCLEO board Uart problem

Posted on March 30, 2015 at 21:45 Hello All, I'm a hobbyst, and recently bought a Nucleo evalboard with STM32L152RE MCU for experimenting the Cortec MCU from ST. I use the free/demo dev environment from keil(MDK V5).I also use the STMCUBE...

and3co by Associate
  • 1528 Views
  • 2 replies
  • 0 kudos

stm32f302 usart interrupt problem

Posted on April 01, 2015 at 03:31 Hi all, I configure my stm32f302's usart without peripheral lib, when i enable it with CR1->UE, the usart interrupt keep triggered and CR1->UEbit cleared automatically, actually i didn't connect anything to RX a...

lijieamd by Associate
  • 1317 Views
  • 2 replies
  • 0 kudos

STM32 General questions

Posted on March 30, 2015 at 11:26Hello, I try to make a demoboard with a STM32F4 controller but I have some problems: Which pins I need to use the stlink programmer from a nucleo board (swdio, swclk ,... )? I found in the datasheet, that some functi...

Timer Interrupt for 1ms

Posted on March 30, 2015 at 14:16I am using STM32F207 VG controller for my learning.I have few following doubts.I want to use timer for up counting.Timer clock is set to 36 MHz.I want to generate timer interrupt for every 1 ms.With what values i nee...

er by Associate II
  • 4589 Views
  • 5 replies
  • 0 kudos

Hardfault Cause on STM32F0xx?

Posted on March 31, 2015 at 13:57Hi, I have tried to find some information about registers signalling the cause of a hard fault  on an STM32F072 but couldn't find anything useful. If anyone could give me some directions I would be glad. Regards, Kil...

STM32F4 Discovery timer syncronization

Posted on March 30, 2015 at 16:46 I am currently trying to generate a squarewave on A8 with TIM1 (50% duty PWM1) and use TIM2 as a slave to trigger an interrupt every 4096th tick (this is used to reset the counter of an LED driver and to push ne...

Leonelf by Associate II
  • 2497 Views
  • 8 replies
  • 0 kudos