STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

(SOLVED) STM32F103C8 UART Interrupt Flooding

Posted on February 07, 2015 at 18:42 Hi I want to receive data from ESP8266 module after restarting it. But after restart, it starts the communication at a higher baud rate and after it's done booting it uses 9600 baud. When I have the UART p...

petoknm by Associate II
  • 1694 Views
  • 1 replies
  • 0 kudos

UART Registers Documentation for STM32F429xx? Where is it?

Posted on April 09, 2015 at 04:40Hi,Where can I find documentation on the UART registers for the STM32F429xx micro?The datasheet ( http://www.st.com/web/en/resource/technical/document/datasheet/DM00071990.pdf ), does not include any information abou...

gustavo23 by Associate II
  • 1020 Views
  • 5 replies
  • 0 kudos

STM32F04 CAN init

Posted on April 09, 2015 at 19:43The original post was too long to process during our migration. Please click on the attachment to read the original post.

SWD connector on custom board

Posted on April 10, 2015 at 18:53Hello, I have a STM32F411 nucleo board and I would like to cut STLink out. I'm building a shield for nuecleo board and I want to add a SWD connector. So I look at CN4 on STLink and  altium schematic and I have some d...

Periodic RTC calibration STM32F1xx

Posted on April 08, 2015 at 15:56Hello,MyProject: Calibrate RTC LSE clock continuously based on an external time reference.MyProblem: Calculation of re-calibration value.Description: I start a calibration measurement interval time t1 and stop it at ...

Function callback on ISR generated by CubeMX

Posted on April 05, 2015 at 00:47Hello, I'm Leonardo, from Argentina.  I've just started with STM32F4 Nucleo board and I'm trying to use CubeMX for Code generation. I configure TIM5 and 4 IC channel to generate Interrupt. So I'm studying the genera...

Internationalization

Posted on April 10, 2015 at 14:24hiwhat is the approach to do  http://askubuntu.com/questions/502987/what-to-do-so-that-issue-net-shows-readable-banner-characters-to-chinese-russian with stm32f4 board?thank #software-design

LIS3DH Accelerometer interrupt to STM32L151

Posted on August 30, 2013 at 00:22I am trying to interface LIS3DH Accelerometer over I2C to STM32l151rx series microcontroller , I am able to Read  X,Y,Z register  content , but i want to use the inbuilt motion detection interrupt feature of LIS3DH ...

akp25i by Associate II
  • 2279 Views
  • 3 replies
  • 0 kudos

STLink Virtual COM Port issues with sending data

Posted on March 23, 2015 at 10:06Hey there, I have a major problem with STM32nucleo an it's virtual COM port. I'm using it for a while to measure some voltages and send them to labview. Sometimes I got the a timeout error in labview, waiting for ser...

STM32F429 SAI HAL_SAI_ErrorCallback errors OVRUDR

Posted on April 10, 2015 at 13:54Hi, i'm using SAI output on STM32F429BIT6. I used some of the code from STM32CubeF4-Example stm324x9i_eval_audio.c for initialization. In pricipal all works fine, but sometimes i get an Error from the SAI interface a...

d239955 by Associate II
  • 658 Views
  • 0 replies
  • 0 kudos