STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F373 Code Question

Posted on April 14, 2015 at 14:05  The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F0 I2C CPAL V2 Listen Mode

Posted on September 26, 2014 at 01:41I am trying to use the CPAL library for I2C communication for the F0 MCU.  This download page seems to suggest that the std peripheral library include CPALv2.  But when I use it, the User manual does not seem to ...

jacky by Associate II
  • 1225 Views
  • 2 replies
  • 0 kudos

STM32F411xx flash latency discrepancy

Posted on April 21, 2015 at 08:32The reference manaul for the STM32F411 series says that for a CPU running at 100MHz on a 2.7-3.6 supply voltage, the flash latency should be 3 wait cycles.  However, the CMSIS startup file (system_stm32f4xx.c v1.5.0...

programming SPI on STM32F091RC

Posted on April 22, 2015 at 17:02Hi everyone, I'm trying to program the SPI2 of my STM32 to only transmit data at 18Mbit/s as I saw on datasheet. My problem is to configure the ''SPI_HandleTypeDef'' in order to use the function : HAL_StatusTypeDe...

raphael by Associate II
  • 702 Views
  • 0 replies
  • 0 kudos

SCCB and I2C problem

Posted on May 24, 2013 at 07:54Hi, I want to interface the OV7670 FIFO omnivision camera with STM32F4discovery board I have used an example inside of  STM32F4xx_DSP_StdPeriph_Lib_V1.1.0, the example drives an OV2640/9655 camera so I changed the regi...

girtor by Associate II
  • 2344 Views
  • 2 replies
  • 0 kudos

DCMI digital camera interface

Posted on November 20, 2013 at 15:14Hi everybody,I'm starting working with image sensors and there is something I don't understand.ST provides a digital camera interface called DCMI. I saw some people are using it OV7670 or OV5642. But in the sensor...

quentin by Associate
  • 1450 Views
  • 3 replies
  • 0 kudos

STM32f407 Discovery 10Mhz Clock Output?

Posted on March 06, 2014 at 10:42I want to use STM32F407 with the OV7670 camera. I need to external 10 MHz clock source.SystemCoreClock 168 MhzAHB Prescaler 1, ABP1 Prescaler 4, ABP2 Prescaler 2Can I get 10 Mhz clock using Timer 3. #stm32f407 #pw...

OV7670 interface cannot get product ID

Posted on July 11, 2012 at 00:52Hi,         I have a problem with interfacing OV7670 camera. I connect only 4 wires from Ov7670 to my stm32f4board, SIO_C, SIO_D, 3V+ and GND. Then I tried to read product id of the camera. It always send 0xFF. I am n...

theparitt by Associate II
  • 2654 Views
  • 6 replies
  • 0 kudos

STM32 port and OV7670 ?

Posted on April 08, 2014 at 04:11 Guys, I have OV7670 module and STM32 dev board, I'm confused on how to connect the port of STM32 and OV7670 at the module because of the name of the port on OV7670 is different with in STM32 code, ...

0690X00000602sPQAQ.jpg