STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 SPI problem

Posted on May 03, 2013 at 09:02I want to interface winbond W25Q64BV SPI flash with STM32F103VE running at 24MHz. I was able to perfectly read the status registers and ID's of flash using commands 0x05,0x35,0x9F,0x4B,0x90,0xAB. But I am not able to e...

CubeMX 4.7.1 not using STM32L1 1.2.0

Posted on May 06, 2015 at 00:27I updated CubeMX and installed the new 1.2.0 firmware for the STM32L1 family earlier today.  However, CubeMX won't migrate existing projects or create new projects using the new firmware package.  Even after deleting 1...

seth by Associate II
  • 1311 Views
  • 2 replies
  • 0 kudos

Confusion on STM32F407 DMA FIFO mode, Please help

Posted on May 04, 2015 at 06:42Hello everyone,Nowadays, I'm trying to figure out how the FIFO of DMA works. But get stumbled with the DMA memory to peripheral mode with FIFO enabled.Firstly, the STM32F4 ''RM0090 Reference manual'' P.219 ''Memory-to-...

sunnyqd by Associate II
  • 5549 Views
  • 10 replies
  • 0 kudos

USB CDC-ECM host implementation

Posted on May 06, 2015 at 14:54Hi,Is there any USB CDC-ECM host implementation example available in ST?This could be a great start to my new project.

vivek1 by Associate
  • 606 Views
  • 0 replies
  • 0 kudos

how to enable Clock-out capability (MCO Pin)

Posted on May 06, 2015 at 13:00I want to have a sample of system clock at MCO pin of STM32F107RC micro controller. I use dspin firmware library for driving stepper motor. The on board crystal is 8MHz and system clock set to be 72MHz. I add this code...

yasamin by Associate II
  • 920 Views
  • 1 replies
  • 0 kudos

SPI Transmit only

Posted on May 05, 2015 at 13:54Hey, I want use the SPI interface of the STM32F407 in transmit only mode. I tried some different solutions but it did not work. Can you tell me please which commands I have to use in the SPI Init? I can not find any op...

gross by Associate II
  • 2007 Views
  • 4 replies
  • 0 kudos

Using SDRAM and NOR Flash

Posted on May 05, 2015 at 09:27I have a simple project running on my STM324x9IEval Kit using external SDRAM and NOR Flash.The project run correctly when a use only SDRAM, &sharpdefine DATA_IN_ExtSDRAM is uncommented in system_stm32f4xx.c and my vars...

ducommun by Associate II
  • 1472 Views
  • 2 replies
  • 0 kudos

STM32f415RG hits reset_handler (Mikroe MINI M4)

Posted on May 06, 2015 at 02:38hi everyone..I bought a MINI M4 from mikroelektronica and I decide to use KEIL 5.04 for the firmware, I ported a proyect from STM32F4DISCOVERY and it seems that it worked, i try the blinking led, push button to turn on...

0690X00000602vCQAQ.jpg 0690X000006031GQAQ.jpg
dracog71 by Associate II
  • 706 Views
  • 0 replies
  • 0 kudos