STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does HAL/Cube support I2C SMB ARP transactions?

Posted on June 19, 2015 at 01:48I'm working with a device that uses the SMB Address Resolution Protocol as part of the response to generating an internal alert. I have no difficulty reading and writing address registers in general (With the peripher...

hbarta2 by Associate III
  • 760 Views
  • 2 replies
  • 0 kudos

Choosing GPIO Speed Setting

Posted on June 19, 2015 at 13:27Hello, what is a sensible relation between the GPIO speed setting and peripheral device speed? E.g. OSPEED = 00 on a >2.7 Volt STM32F42x with 10 pF load has a value of 8 MHz max. Is that good for a SPI clock rate of 8...

ST-LINK_CLI with win7

Posted on June 15, 2015 at 10:20Hi,I noticed that when i'm trying to flash via the ST-Link_CLI in win 7 when i'm administrator.the response that i'm getting from the ST-Link_CLI is ''Unable to open file!''but when i'm doing it  without setting my se...

STM32F303VC ADC+DMA problem

Posted on June 18, 2015 at 18:04The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F303VCT6 running ISR from ccmram

Posted on June 18, 2015 at 22:06Hi, I have been trying to run critical interrupt routines from ccmram with gcc toolchain following the instructions in http://www.st.com/web/en/resource/technical/document/application_note/DM00083249.pdfI think I have...

eirik by Associate II
  • 1863 Views
  • 4 replies
  • 0 kudos

Is it possible to wirelessly upload program to the CPU?

Posted on June 18, 2015 at 16:54In one project there is a large rotating machine. It would help a lot if programs could be uploaded wirelessly(, while the motor is on). We would like to do other things, so doing our own solution is not good idea. It...

LMI2 by Lead
  • 2285 Views
  • 7 replies
  • 0 kudos

IAP ISSUE

Posted on January 10, 2014 at 04:14Working on STM32F051. The bootloader works fine but the interrupt vectors in application file doesn't work even after locating vector table to SRAM. Any solution will be appreciated.

VTOR does not work when ROM is loaded from 0x8003000

Posted on June 18, 2015 at 11:41Hello,I have written own bootloader/IAP that should start next firmware (jump to it).It is working very well, but when the firmware is loaded, then interrupts are not working.Of course I have configured:#define VECT_T...

zexx86 by Associate II
  • 1206 Views
  • 3 replies
  • 0 kudos