Skip to main content
leosad
Associate II
November 7, 2014
Question

USART Problem with nucleo L152

  • November 7, 2014
  • 6 replies
  • 1401 views
Posted on November 07, 2014 at 12:41

Hello!

I'vegot an issue with using USART on Nucleo L152LE and need some help. Symptoms are: RX and TX pins are hardware connected, but reading from input register with USART_ReceiveData(USART1) returns zero instead of transmitted value. IDE is Atolic Lite with project settings coresponding to used board. I've tried both USART1 (PIO A, pins 9 and 10) and USART2 (PIO A, PINS 2 and 3) with the same result.

Here is initialization code for USART1:   

/* USART configuration structure for USART1 */

    USART_InitTypeDef USART1_init_struct;

    /* Bit configuration structure for GPIOA PIN9 and PIN10 */

    GPIO_InitTypeDef gpioa_init_struct;

USART_ClockInitTypeDef  USART_ClockInitStructure;

    USART_ClockStructInit(&USART_ClockInitStructure);

USART_ClockInit(USART1, &USART_ClockInitStructure);

     

    /* Enable clock for USART1, AFIO and GPIOA */

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

    /* GPIOA PIN9 alternative function Tx */

    gpioa_init_struct.GPIO_Pin = GPIO_Pin_9;

    gpioa_init_struct.GPIO_Speed = GPIO_Speed_40MHz;

    gpioa_init_struct.GPIO_Mode = GPIO_Mode_AF;

  gpioa_init_struct.GPIO_OType = GPIO_OType_PP;

    gpioa_init_struct.GPIO_PuPd=GPIO_PuPd_DOWN;

    GPIO_Init(GPIOA, &gpioa_init_struct);

    

    /* GPIOA PIN10 alternative function Rx */

    gpioa_init_struct.GPIO_Pin = GPIO_Pin_10;

    gpioa_init_struct.GPIO_Speed = GPIO_Speed_40MHz;

    gpioa_init_struct.GPIO_Mode = GPIO_Mode_IN;

    gpioa_init_struct.GPIO_PuPd=GPIO_PuPd_DOWN;

  gpioa_init_struct.GPIO_OType = GPIO_OType_PP;

    GPIO_Init(GPIOA, &gpioa_init_struct);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource9|GPIO_PinSource10, GPIO_AF_USART1);

    /* Baud rate 9600, 8-bit data, One stop bit

     * No parity, Do both Rx and Tx, No HW flow control

     */

    USART1_init_struct.USART_BaudRate = 9600;

    USART1_init_struct.USART_WordLength = USART_WordLength_8b;

    USART1_init_struct.USART_StopBits = USART_StopBits_1;

    USART1_init_struct.USART_Parity = USART_Parity_No ;

    USART1_init_struct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    USART1_init_struct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    /* Configure USART1 */

    USART_Init(USART1, &USART1_init_struct);

    /* Enable USART1 */

    USART_Cmd(USART1, ENABLE);

    /* Enable RXNE interrupt */

//    USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);

/*    

    NVIC_EnableIRQ(USART1_IRQn);

*/    

}

And transmittion code:

int  UartWriteWithEcho(unsigned char *pBuf,unsigned DataLen)

{

unsigned cnt;

uint16_t RetVal;

for(cnt=0; cnt<DataLen; cnt++)

{

USART_SendData(USART1, pBuf[cnt]);

while (USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET)

{

//Do nothing. Just wait

}

RetVal=USART_ReceiveData(USART1);

if( (unsigned char)RetVal!= pBuf[cnt]) //Checking echo is correct

return 0;

}

return 1;

}

Would anyone be so kind to point me what is wrong?

#nucleo-stm32l152-uart-txe #nucleo-stm32le-usart-problem
This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
November 7, 2014
Posted on November 07, 2014 at 15:50

I've posted SPL examples for the L1 Nucleo

GPIO_PinAFConfig(GPIOA, GPIO_PinSource9|GPIO_PinSource10, GPIO_AF_USART1); // Doesn't work like this, won't OR together

Use TXE to see if the register is empty, NOT TC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
leosad
leosadAuthor
Associate II
November 7, 2014
Posted on November 07, 2014 at 16:52

Thank you for response.

Unfortunately these changes didn't help

Tesla DeLorean
Guru
November 7, 2014
Posted on November 07, 2014 at 17:18

// STM32 USART2 (Tx PA.2, Rx PA.3) STM32L152RE NUCLEO - sourcer32@gmail.com
#include ''stm32l1xx.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
/* GPIOA clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; // PA.2 USART2_TX, PA.3 USART2_RX
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);
}
/**************************************************************************************/
void USART2_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_Cmd(USART2, ENABLE);
}
/**************************************************************************************/
void OutString(char *s)
{
while(*s)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, *s++); // Send Char
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART2_Configuration();
OutString(''Welcome to Nucleo L152RE

'');
while(1) // Don't want to exit
{
uint16_t Data;
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); // Wait for Char
Data = USART_ReceiveData(USART2); // Collect Char
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, Data); // Echo Char
}
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d

'', file, line) */
while (1)
{}
}
#endif
/**************************************************************************************/

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
November 7, 2014
Posted on November 07, 2014 at 17:23

Quick blind mod, presupposes PA9/PA10 are conflict free, HSE_VALUE is correct, and being connected to a CMOS Serial adapter, the voltages here are not RS232 compatible levels.

// STM32 USART1 (Tx PA.9, Rx PA.10) STM32L152RE NUCLEO - sourcer32@gmail.com
#include ''stm32l1xx.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* GPIOA clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; // PA.9 USART1_TX, PA.10 USART1_RX
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1);
}
/**************************************************************************************/
void USART1_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
/**************************************************************************************/
void OutString(char *s)
{
while(*s)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART1, *s++); // Send Char
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART1_Configuration();
OutString(''Welcome to Nucleo L152RE

'');
while(1) // Don't want to exit
{
uint16_t Data;
while(USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET); // Wait for Char
Data = USART_ReceiveData(USART1); // Collect Char
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART1, Data); // Echo Char
}
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d

'', file, line) */
while (1)
{}
}
#endif
/**************************************************************************************/

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
leosad
leosadAuthor
Associate II
November 18, 2014
Posted on November 18, 2014 at 08:58

Thank you a lot! It works, although with one notice - RX pin also need to be set in AF mode. Without this where are no incoming data at all.

Next problem is - if I use TXE flag in transmittion remote end gets wrong data... Looks like a mix of previous and next symbol. I think where are a kind of problem with UART clock settings, but I'm not sure. Can you point me to possible reasons? 

Tesla DeLorean
Guru
November 18, 2014
Posted on November 18, 2014 at 14:25

If the receiver has problems with inter-symbol separation you could try 2 stop bits.

TXE flags that the holding register is empty, TC is more useful to know when the last bit of the last byte has left the USART
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..