cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 configure TIMER2 for 1microsec interrupt

hariprasad
Associate III
Posted on November 10, 2014 at 15:14

Hi

I want to generate a timer interrupt after every 1micoseconds. I am using TIMER2 for this purpose.So I took a code from one site and modified for my purpose.

But the issue is I cant get an interrupt of 1microsecond.To ensure this I toggled a gpio in the ISR and verified the frequency on DSO and it was found to be 806Khz.

Is there anything that I'm doing wrong in the code?

void TIM2_IRQHandler(void)

{

  if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)

  {

        count++;

      TIM_ClearITPendingBit(TIM2, TIM_IT_Update);

        flag_for_state_machine=1;

        if(count%2 == 0)

            GPIO_ResetBits(GPIOD, GPIO_Pin_12);

        else

            GPIO_SetBits(GPIOD, GPIO_Pin_12);

  }

}

void configure_d1_d2_d3(void)

{

        /* Enable the GPIO_LED Clock */

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

}

void INTTIM_Config(void)

{

  NVIC_InitTypeDef NVIC_InitStructure;

  /* Enable the TIM2 gloabal Interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

  /* TIM2 clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);    

  /* Time base configuration */

  TIM_TimeBaseStructure.TIM_Period = 1;

  TIM_TimeBaseStructure.TIM_Prescaler = 0;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

  /* TIM IT enable */

  TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);

  /* TIM2 enable counter */

  TIM_Cmd(TIM2, ENABLE);

}

int main(void)

{    

        configure_d1_d2_d3();

        INTTIM_Config();

        while(1);        

}

#discovery #stm32f4 #timers
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on November 10, 2014 at 15:47

Interrupting at 1 MHz is ridiculously fast, think a bit harder about a better way to solve whatever problem you are trying to solve.

TIM_TimeBaseStructure.TIM_Period = 1; // Like 84 MHz / 2? WTF?

TIM_TimeBaseStructure.TIM_Prescaler = 0;
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 10, 2014 at 15:51

TIM_TimeBaseStructure.TIM_Period = ((SystemCoreClock / 2) / 1000000) - 1;  // 1 MHz (1us)

Toggling will HALF the measured frequency. So if the interrupt occurs at 1 MHz (1 us) the pin frequency will be 500 KHz
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
stm322399
Senior
Posted on November 10, 2014 at 15:59

IMHO, you should ask yourself how to execute the following under 1us:

void TIM2_IRQHandler(void)
{
if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
{
count++;
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
flag_for_state_machine=1;
if(count%2 == 0)
GPIO_ResetBits(GPIOD, GPIO_Pin_12);
else
GPIO_SetBits(GPIOD, GPIO_Pin_12);
}
}

What about having a look at assembly code ? Then try to follow the flow or count instructions (beware 1 instruction may require more than one cycle). Clive is right, there are very few use case that requires to go at that rate. What do you try to achieve ? Maybe it could be done in an other way (DMA ?).
hariprasad
Associate III
Posted on November 18, 2014 at 05:37

Hi Clive,

Thanks for the reply, that worked

If I want to generate interrupt at 2 Mhz (0.5microsec) How should I modify the above program?

Posted on November 18, 2014 at 15:09

If this wasn't evident from the previous example:

TIM_TimeBaseStructure.TIM_Period = ((SystemCoreClock / 2) / 2000000) - 1;  // 2 MHz

You should really let the hardware do the toggling at these rates, it's not a viable rate to interrupt at, and at some point you will saturate the processor.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..