STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI FLASH read/write problem

Posted on July 21, 2013 at 13:50 Hello, i am making adsp-21488 spi flash programmer, and i run into some trublmes. I use STM32F415 and using SPI1 (PA5/6/7) *** PB0 for communication with SPI. I can read Flash ID with no problem, and it's...

_legacyfs_online_stmicro_images_0690X00000604zb.png

OV7670 with stm32f4-discovery?

Posted on January 11, 2013 at 18:51I have a project with OV7670 with stm32f4-discovery. My OV7670 has 16 pins and without fifo. And I don't have LCD. I hope I can use OV7670 to get view into stm32f4 and transmit data to smart phone and get the real ...

ctc.ctc by Associate II
  • 2141 Views
  • 5 replies
  • 0 kudos

OV7670 camera

Posted on February 15, 2012 at 08:55Good day,I have some problem here, I took some code from another project, I rewrote some parts. But my camera do not want to work. I just want to read the ID of camera through I2C (or so called SCCB), but I always...

hitsumen by Associate II
  • 2736 Views
  • 4 replies
  • 0 kudos

UNUSED PINS OF A PERIPHERAL

Posted on June 27, 2015 at 00:51Hi, when I use a peripheral with some unused pins, can I use other alternate functions of those pins (for other peripherals)? for example, in STM32f407, I use SPI2 with unused SPI2_NSS (pin 140). can I use this pin as...

Can't connect to Discovery card

Posted on June 27, 2015 at 17:52Just after I downloaded a program into Stm32F100 Discovery card, the STM32 ST-LINK Utility lost contact with the card. Now it cannot connect to it, no matter what I do. The software in the card is a plain GPIO test fr...

LMI2 by Lead
  • 1563 Views
  • 3 replies
  • 0 kudos

STM32F401RE Firmware update over Bluetooth

Posted on June 27, 2015 at 16:05Hi, i got a Nucleo F401RE Board and tried to update the flash with the internal bootloader, it works perfectly with USB<->RS232 bridge at 115200baud on UART1 (PA9,PA10), i got correct responses from bootloader, id, an...

sauer by Associate II
  • 1542 Views
  • 2 replies
  • 0 kudos

CAN RX IRQ Question STM32F429

Posted on June 27, 2015 at 19:16 //---------------------------------------------------------------------------- setup CAN interface *----------------------------------------------------------------------------*/ void CAN_setup (uint32_t ctrl) { C...

Programming Bare STM32F0 Chip with Discovery SWD

Posted on June 18, 2015 at 12:57I have programmed many STM32F030C8 chips with Discovery board but the success rate while trying to program each Chip is very low. Some times after many tries the chip gets programmed and some times it does not work at...

audio_playback_and_record example add uart2

Posted on June 26, 2015 at 20:36audio_playback_and_record example add uart2 hello everyone. this week i start to dev in stm32f4discovery install cubeMX and get examples STM32Cube_FW_F4_v1.6.0 edditing audio_playback_and_record example  and add uart...