Skip to main content
hussnain_sal
Associate
November 29, 2014
Question

dead time in stm32f4

  • November 29, 2014
  • 2 replies
  • 1585 views
Posted on November 29, 2014 at 17:24

I'm generating a 50Hz complementary PWM wave in stm32f4 i'm stuck on dead-time insertion as i want to insert a dead time of 2.5ms, I don't know how to do that here is my code. This is what I thought it should be but results are not accordingly ..

 

  /* Compute the value to be set in ARR register to generate signal frequency at 50 Hz */

  TimerPeriod = (10000 / 50) - 1; // ARR = 199

  /* Compute CCR1 value to generate a duty cycle at 50% for channel 1 */

  Channel1Pulse = (uint16_t) (((uint32_t)50 * (TimerPeriod - 1)) / 100);

  /* Time Base configuration */

  TIM_TimeBaseStructure.TIM_Prescaler = 1679; // TO set counter at 10Khz

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseStructure.TIM_Period = TimerPeriod;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;

  TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

  /* Channel 1 Configuration in PWM mode */

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;

  TIM_OCInitStructure.TIM_Pulse = Channel1Pulse;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;

  TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;

  TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;

  TIM_OC1Init(TIM1, &TIM_OCInitStructure);

  /* Automatic Output enable, Break, dead time and lock configuration*/

  TIM_BDTRInitStructure.TIM_OSSRState = TIM_OSSRState_Enable;

  TIM_BDTRInitStructure.TIM_OSSIState = TIM_OSSIState_Enable;

  TIM_BDTRInitStructure.TIM_LOCKLevel = TIM_LOCKLevel_1;

  TIM_BDTRInitStructure.TIM_DeadTime = 25; //2.5ms for the case of 10Khz counter clock 25/10000 = 0.0025 sec = 2.5ms

  TIM_BDTRInitStructure.TIM_Break = TIM_Break_Enable;

  TIM_BDTRInitStructure.TIM_BreakPolarity = TIM_BreakPolarity_High;

  TIM_BDTRInitStructure.TIM_AutomaticOutput = TIM_AutomaticOutput_Enable;

  TIM_BDTRConfig(TIM1, &TIM_BDTRInitStructure);

#dead-time #stm32f4 #pwm
This topic has been closed for replies.

2 replies

diego2
Visitor II
November 29, 2014
Posted on November 29, 2014 at 21:47

are you using the old std peripheral driver library?, because i have an example with the new stm32cubef4 library. Are you interested?

hussnain_sal
Associate
November 30, 2014
Posted on November 30, 2014 at 11:21

Ya sure I'll be grateful if you help by sharing your work