STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using SD Card with STM32L152C Discovery

Posted on July 08, 2015 at 09:25I have a STM32L152C Discovery board. I want to use a 1GB FAT SD Card with STM32Cube and EWARM ide, but there is an error. pins:     STM --- SD Module     PA5       SCK     PA4       CS     MISO    MISO     MOSI    MOS...

babak by Associate
  • 655 Views
  • 0 replies
  • 0 kudos

How to use 30Mhz clock on SPI SCK.

Posted on July 08, 2015 at 08:14I'm using stm32f429. I have configured my system core clock to 160Mhz and I use the APB2 clock divider as 4, which gives me 40Mhz to my SPI4 peripheral , I want to use my SPI peripheral at 30Mhz, since the SPI core cl...

too high value on one channel adc

Posted on July 06, 2015 at 14:20 hi everybody! I'm developing on st32f0 a device with two analogics sensors. After the initialization, I can read properly one value but the other is always at it s maximum value (4095 for 12 bits of data). ...

STM32F427 Inverted DAC output

Posted on July 07, 2015 at 20:13I've seen at least two other threads with an inverted DAC concern being present, wondering if anyone has more information o the issue? I have 3 identical boards in house populated with the F4, one of which has an inve...

STM32F407VET PLL problem

Posted on July 07, 2015 at 17:00 I used STM32 cube for the PLL configuration // Enable HSE Oscillator and activate PLL with HSE as source RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_...

kareemkna by Associate II
  • 3588 Views
  • 11 replies
  • 0 kudos

4 channel frequency measurement on a single timer

Posted on July 07, 2015 at 18:18I've been testing a STM32F4 Discovery since I'm new to ST Microcontrollers and I wanted to use one timer to measure 4 different channel frequencies, as I want to measure more signals than there are timers. I do not ca...

0690X00000605XPQAY.png 0690X00000605JSQAY.png 0690X00000605XeQAI.png
jackygip by Associate II
  • 1742 Views
  • 2 replies
  • 0 kudos

Optimization in CooCox on an STM32F415VG

Posted on July 07, 2015 at 11:49Hi guys, I have code that has been working great for a couple of months now on an STM32F415VG, but I added some libaries/code yesterday which took it beyond the flash sectors that I wanted it to sit in (it's a custom ...

Timer Interrupt for UART communication

Posted on July 07, 2015 at 09:47 Hello, I want STM32 with GSM board each sec communicate. in Main.c int main(void) { HAL_Init (); SystemClock_Config (); HARD_LED_Init(LED_GREEN); Term_UART_Config(); HARD_TIM_Init(); while (1) ...

astree by Associate II
  • 2231 Views
  • 4 replies
  • 0 kudos

Sharing functions between two pieces of code

Posted on July 07, 2015 at 16:27My subject doesn't quite describe what I'm trying to do, but not quite sure how else to explain: I have a bootloader stored at the start of flash in my STM32f415 (flash location 0x08000000), and my main application is...