User Activity

Hello, I am testing two STM32WL55. I have two NUCLEO-WL55JC2 demoboards. I'm using the example code provided in the LocalNetwork_Concentrator and LocalNetwork_Sensor demos. In the basic configuration, I cannot manage to have a communication distance ...
Hello,I have bought a devkit NUCLEO-WL55JC2. I'm looking for an IAR EWARM template project or examples. Someone knows where i can find it? I find only examples running under CUBEIDE.Thanks !:grinning_face:
Hello,We are designing a PCB based on the NUCLEO-WL55JC boardWe are looking for the Altium project files.Someone can share a link?Thanks.BEEPH
Posted on February 08, 2015 at 23:36Hello, I'm using IAR EWARM 6.70.1.5794 for developping a firmware on a STM32F107VCT6. I use a ST LINK V2 for debug. Now i would like generate an hex or bin file for downloading the file without ST-LIN V2 but with ...
Kudos from