STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nice problem with IAR ARM Compiler

Posted on August 04, 2015 at 09:40 So many of you know i am having hard time to make my STM32F4 program work with STM32F7 micro. Latest finding for me looks just not acceptable. So many people to make programs shorted use function calls ...

STM32F1x(/4x?) SDIO DMA TX FIFO underruns

Posted on August 04, 2015 at 23:32As many others on the forums and the Interwebs have, I recently ran into a problem with SDIO TX FIFO underruns, even when using DMA at the highest priority.  I did figure out a solution though, and thought I would s...

Feedback/issues in Cube app V4.7.0

Posted on April 27, 2015 at 05:59Few things I've found with the Cube Generator app V4.7.0:- in the I2C configuration section, the maximum clock speed is 100 khz, even if Fast Mode is selected. Can't select 400 khz- in the LwIP options, it seems that...

[STM32F4 Discovery] Can't breakpoint in RTC ISR

Posted on August 05, 2015 at 02:17 Hi all, I am evaluating STM32F4 Discovery board. I have quite a strange problem that I don't really understand. I generated a project via the STMCube software (no changes to the default discovery board confi...

jitesh by Associate
  • 828 Views
  • 0 replies
  • 0 kudos

STM32F7 UART HAL Driver Bug

Posted on August 04, 2015 at 22:58The STM32F7 HAL Driver (v1.1.0) has a bug in the __HAL_UART_CLEAR_IT macro:Writing a bit to the ICR register clears the corresponding interrupt; however the __HAL_UART_CLEAR_IT writes the ones-complement:&sharpdefin...

malcolm23 by Associate III
  • 1952 Views
  • 1 replies
  • 0 kudos

STM32F103 - DAC

Posted on August 02, 2015 at 14:00Hi dear friends,I have the SMT32F103RCT6 and I trying to use the DAC with DMA. I compile the ''OneChannelDMA_Escalator'' example and unfortunately it won't work, When I change the code so it will work without the DM...

jaykov by Associate II
  • 6310 Views
  • 10 replies
  • 0 kudos

STM32F427 UART DMA Receive Problem

Posted on August 04, 2015 at 21:23The original post was too long to process during our migration. Please click on the attachment to read the original post.

hal by Associate
  • 1387 Views
  • 1 replies
  • 0 kudos

ITM, Debug window,CMISIS support

Posted on August 04, 2015 at 17:46HelloI am using NUCLEO L053R8 (STM32L0) and Keil uVision 5.15 and ST-Link (embedded in the nucleus board). I buid a FW program using CubeFx I am setting up the stdoutput with no semihosting using the ITM.First I can...

stanzanim by Associate III
  • 1365 Views
  • 3 replies
  • 0 kudos

__ADCX_FORCE_RESET() not seen

Posted on August 03, 2015 at 16:58 I am using the version 1.3.1. of stm32f4xx hal drivers. I am using the 3 ADCs. ADC1 and ADC2 in dual mode DMA interrupt driven and ADC3 regular conversion. As you can in the code below I am using the fun...

keaven by Associate II
  • 1163 Views
  • 4 replies
  • 0 kudos