STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using templates with IAR

Posted on August 25, 2014 at 03:29Hi everyone,So i have started to use STM32 MCUs.I used before Tiva MCUs with IAR and now i'm trying it with the ST.I realy find hard to configure a project to work with the HAL drivers. You need always do so much ea...

luis by Associate II
  • 2334 Views
  • 4 replies
  • 0 kudos

STM32F3 ADC-DMA restarting

Posted on August 06, 2015 at 14:24 Hello! I configured the ADC with DMA to fill a table in RAM. After ADC_StartConversion (ADC1); I use while (!DMA_GetFlagStatus (DMA1_FLAG_TC1)) ; until the DMA is full. This works fine for one...

STM32F3 Flash page capacity and reading from Flash

Posted on August 04, 2015 at 13:24Hello, Lately I've been trying to save some data on flash in my STM32F3 discovery board. Saving data was succesful but I have a little problem in reading from this memory. Function I'm using to check my data is:  ui...

dooz by Associate II
  • 1824 Views
  • 4 replies
  • 0 kudos

STM32F3 programming flash writing (missing function)

Posted on July 29, 2015 at 15:09Hello, Recently I've been trying to configure writing to flash memory in STM32F3 discovery. I'm using STM32CubeMX and System Workbench for STM32. I've read many guides how to do it and example codes so I guess I alrea...

dooz by Associate II
  • 1210 Views
  • 3 replies
  • 0 kudos

Bug in HAL library (HAL_RTCEx_SetWakeUpTimer_IT)

Posted on August 01, 2015 at 18:18*Bug: HAL_RTC weakup does not interrupt*Reason:  The library  stm32f4xx_hal_rtc_ex.h  missing to clear the interrupt flag before enabling the interrupt *Solution: Manually add this line (clear the interrupt flag): /...

EXTI IRQ vs EVENT

Posted on August 06, 2015 at 08:08Hello,I don't know if this was already discusses somewhere, but what is main difference between EXTI interrupt and event mode? I understand that in EVENT mode IRQ is not called or similar, but how to handle events?I...

tm3341 by Associate II
  • 4578 Views
  • 2 replies
  • 0 kudos

STMN32F407 TIM5 UIF interrupts

Posted on August 05, 2015 at 19:55Hello: I am using a stm32F407 and working on getting the timer overflow working correctly and I am seeing a strange thing. Basically, I seem to be getting two TIM5 interrupts for each overflow of the counter. Nothin...

will by Associate II
  • 2285 Views
  • 5 replies
  • 0 kudos

STM32F4 Discovery program for moving Dynamixel

Posted on August 05, 2015 at 08:11Hello, I am a college student and a beginner programmer, I got a project to make a library using STM32F4 Discovery to move a Dynamixel motor type XL-320. I already studied the basic communication for commanding Dyna...

itsna_azz by Associate II
  • 1661 Views
  • 2 replies
  • 0 kudos

ST32 desvovery IAR tool issue

Posted on August 06, 2015 at 04:53Hi, I'm new here and not sure if it okay to ask this kind of questoin in this place. But it would be great if someone has an answer. Recently I got STM32-discovery and tested some examples on IAR Embedd d workbench....