STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube and #define USE_HAL_DRIVER...

Posted on August 20, 2015 at 09:16Hi,I'm using cube with HAL driver.. and need your help to understand the right way to include headers.I do not understand this example:I includes ''stm32f4xx_hal_adc.h'' ''stm32f4xx_hal_adc.h'' includes ''stm32f4xx_...

samuel23 by Associate III
  • 3659 Views
  • 4 replies
  • 0 kudos

Cube/MX frustration

Posted on August 05, 2015 at 23:18Hi STM32Cube/MX users,I've been using Stm32_StdPerihLib for years in dozens of successful projects. Now, after ST decided to replace SPL wir Cube I was ready to give it a try.My first impression was very positive - ...

osama2 by Associate II
  • 3311 Views
  • 7 replies
  • 1 kudos

Standarddeviation using DSPLib returns 0

Posted on August 19, 2015 at 15:02Hi,I have encountered the following problem on the STM32F4 using the CMSIS DSP Library V1.4.2:When calculating the standard deviation using arm_std_f32() of the following values </colgroup> 7111.15283 7111.3867...

USART DMA transmission

Posted on August 20, 2015 at 11:49Hello,i'm using the HAL library and CubeMx. The chip is a STM32F334C8.I want to send datas on USART1 with DMA control. The datas are well sent but when i go to the DMA complete transfer interrupt, i wait in the inte...

STM32F0 Nucleo(F070RB) board bootloader

Posted on August 19, 2015 at 13:09Hi, I am trying to connect to the bootloader on nucleo -F070Rb board. I tried the Flash loader Demonstrator, but I get ''No response from the target...''. I tried to send the start comman byte (0x7F) using realterm ...

seed by Associate III
  • 1896 Views
  • 4 replies
  • 0 kudos

Reconfiguring a Timer within its interrupt handler

Posted on August 18, 2015 at 20:59 On an STM32F4 Discovery (STM32F407) I'm trying to set up a timer and then reconfigure it within its own interrupt handler. The idea is that I should be able to repeatedly trigger tasks from the ISR in an...

quad_spi interface in F7 microcontrollers

Posted on August 20, 2015 at 09:14Hello. I'd like to know what microcontrollers has qspi interface? Whole STM32F7 series? The document DS10916 says that ''All STM32F75xx devices embed a Quad SPI memory interface, ...''(2.9.Chapter) but there is  no ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.