STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change PWM pulse

Posted on September 14, 2015 at 20:00 Hi, I'm using a servo with a pwm connection and this is a part of code: RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_1); GPIO_InitTypeDef GPI...

fenice-6 by Associate II
  • 976 Views
  • 1 replies
  • 0 kudos

PWM change not initially happening

Posted on September 14, 2015 at 16:40Hello Everybody.I am observing some strange behavior on the scope for a PWM output. I am driving it at 800kHz with alternating high time of 400ns and 800ns.In the TIM1_UP_TIM10_IRQHandler I am alternating the hig...

mlickess by Associate II
  • 1559 Views
  • 4 replies
  • 0 kudos

STM32 not restart after external Reset

Posted on September 07, 2015 at 11:10 Dear all I use a master uP (STM32F072R8) and a slave uP (STM32F030K6) The slave processor is in AC main voltage and the main processor is galavanic isolated from main voltage. The main processor can rese...

franz2 by Associate III
  • 878 Views
  • 1 replies
  • 0 kudos

Uart in 7bit mode

Posted on September 12, 2015 at 15:51I'm using STM32F051R8 board but i'm unable to configure UART in 7bit bata and one bit parity mode. Tried changing M and PCE bits of UART CR1 register but no luck.

Checksum Error after download Firmware PackageSTM32F4 1.8.0

Posted on September 01, 2015 at 12:39after download the Firmaware Package STM32F4 1.8.0 with STM32CubeMX Version 4.10.0, an error occurs: stm32cube_fw_f4_v180.zip (MD5 file checksum is not good). It tried it several times on different PC's with the ...

owl_bo by Associate
  • 1912 Views
  • 4 replies
  • 0 kudos

Stm32f103c8 - clock configuration issue

Posted on September 14, 2015 at 13:36 Hello all, i started working with a small stm32f103c8t6 (medium size device) which i want to use it without any external crystal, so i configured it with usage of internal HSI oscilator. From wha...

Bogdan by Senior
  • 1488 Views
  • 2 replies
  • 0 kudos

Starting with STM32F0DISCO...''errors''

Posted on September 14, 2015 at 12:25Hi, i'm just start working with the Discovery Board STM32F072B. I've installed CubeMX, the MDK-ARM 5.16a & ST-Link Utility 3.7.0 At first i want to go through the examples of the Disco-Board. I can start and rebu...

fbrand by Associate
  • 1038 Views
  • 2 replies
  • 0 kudos

TIM1 update interrupt not firing.

Posted on September 11, 2015 at 13:11Hello Everybody.I am having trouble with the output compare function of an STM32F401RE. I am testing the OC function to generate a waveform by toggling an output at the compare point and the overflow point.The co...

mlickess by Associate II
  • 1947 Views
  • 1 replies
  • 1 kudos

DMA fifo algorithm for non regular data

Posted on September 13, 2015 at 23:14Hello I am trying to figure out DMA and write buffer for incoming TCP data to send over USART I was thinking about using circular DMA (for USART TX) and  add data to buffer. When new data arrives stop DMA and add...

ADC's EOC event

Posted on November 19, 2012 at 13:29Hello, everyone!I have a question about ADC's EOC event, when is this bit been set?For example,there are 6 ADC channels in my program.Is it right as bellow:A channel converted--EOC--B channel converted--EOC...F ch...

icuic by Associate
  • 4040 Views
  • 6 replies
  • 0 kudos