Skip to main content
kasun_duminda92
Associate II
January 1, 2013
Question

PWM signal generation for a servo motor

Posted on January 01, 2013 at 14:08

I want to generate a PWM signal to control a servo motor. The servo has a dead band width of 10?s. I have tried doing this using the '7_PWMOutputs' example.

Code so far:

_______________________________________________________________________

TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

TIM_OCInitTypeDef  TIM_OCInitStructure;

uint16_t TimerPeriod = 0;

uint16_t Channel1Pulse = 0,

GPIO_InitTypeDef GPIO_InitStructure;

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_2);

TimerPeriod = (SystemCoreClock / 17570) - 1;

/* With variable 'x'*/

Channel1Pulse = (uint16_t) (((uint32_t) 25 * (TimerPeriod - 1)) / 100);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 , ENABLE);

TIM_TimeBaseStructure.TIM_Prescaler = 0;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseStructure.TIM_Period = TimerPeriod;

TIM_TimeBaseStructure.TIM_ClockDivision = 0;

TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;

TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;

TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;

TIM_OCInitStructure.TIM_Pulse = Channel1Pulse;

TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High;

TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;

TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;

TIM_OCInitStructure.TIM_Pulse = Channel1Pulse;

TIM_OC1Init(TIM1, &TIM_OCInitStructure);

TIM_OCInitStructure.TIM_Pulse = Channel1Pulse;

TIM_OC1Init(TIM1, &TIM_OCInitStructure);

TIM_Cmd(TIM1, ENABLE);

TIM_CtrlPWMOutputs(TIM1, ENABLE);

while(1){

}

_______________________________________________________________________

How and where should I change or what should I add more to output a PWM signal with a 25% duty cycle and a 10?s dead band width.

Thanks in advance!

#pwm
This topic has been closed for replies.

7 replies

Tesla DeLorean
Guru
January 1, 2013
Posted on January 01, 2013 at 19:30

The PWM Frequency is controlled by the Prescale and Period values, divided into the timer source clock, the width is controlled by Pulse in units in the range of the Period value, and quanta of timer source divided by Prescale.

Prescale and Period are in the form N-1, where N is the divisor.

Here is a 50 Hz Servo example for the VL Discovery, I have something similar for the F4

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Servo%20control%20using%20STM32VLDiscovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51&currentviews=1106]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32VLDiscovery%2FServo%20control%20using%20STM32VLDiscovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51¤tviews=1106
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rihab150192
Visitor II
May 16, 2014
Posted on May 16, 2014 at 18:18

Tesla DeLorean
Guru
May 16, 2014
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rihab150192
Visitor II
May 16, 2014
Posted on May 16, 2014 at 22:40

Thank you for the code but it didn't work i use microservo TowerPro 9g and it has only one input 

Tesla DeLorean
Guru
May 16, 2014
Posted on May 17, 2014 at 00:45

Thank you for the code but it didn't work i use microservo TowerPro 9g and it has only one input

Then just use one output.... If you think there is a problem with the signal inspect it with a scope and report.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
lee2
Visitor II
April 13, 2015
Posted on April 13, 2015 at 21:05

lee2
Visitor II
April 13, 2015
Posted on April 13, 2015 at 21:08