STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CS42L52 i2s

Posted on September 26, 2015 at 18:36Hi All,I am working on MCBSTM32C board and I want to make the CS42l52 work. I tried but seems the DMA is not working. I upload my code. Could someone please help me? #mcbstm32c #stm32f107 #cs42l52

fangdu by Associate II
  • 979 Views
  • 1 replies
  • 0 kudos

SVC_Handler fails badly - hardfaults

Posted on September 06, 2013 at 19:20Below is the code for asm SVC handler straight from an example by ARM: SVC_Handler     STMFD        sp!,{r0-r3,r12,lr}          ; Store registers.   LDR          r0,[lr, #4]                        ; Calculate add...

denis by Associate II
  • 3541 Views
  • 10 replies
  • 0 kudos

STM32F7 - Can not write to FPB registers

Posted on September 25, 2015 at 21:56Hi All, During conversion of our debugging code from Cortex-M3/M4 to M7 I run into following problem - it seems that it is not possible to write to any registers in FPB unit, for example FP_CTRL (0xE0002000) or F...

branislav by Associate II
  • 2439 Views
  • 4 replies
  • 0 kudos

F2/F4 Security against reverse engineering

Posted on September 28, 2015 at 21:58There are facilities in china where you can hire resources for 200 US dollars an hour to reverse engineer microprocessors even if the flash protection bits are set or fuses blown - for example one technique is to...

estersci2 by Associate III
  • 4022 Views
  • 7 replies
  • 0 kudos

USART1 Doesn't transmit

Posted on September 28, 2015 at 21:10I have been trying to get my code to work but I cannot get any output on PA9 (USART1_Tx) on my STM32f0discovery board. Any help would be greatly appreciated. CODE =================================================...

mblack by Associate II
  • 1534 Views
  • 4 replies
  • 0 kudos

Measuring time on STM32f401

Posted on September 29, 2015 at 11:52 hi, I'm trying to turn ON and OFF the LEDs of my board with 10-second intervals, but I get results in about 8 seconds. This is my code, I did not understand the frequencies of the processor card. I apo...

JLink is not able to detect STM32L476

Posted on August 26, 2015 at 16:50 We are using STM32L476 Eval board and J-Link Cortex-M JLink_V499a We flashed the FreeRTOS_LowPower provided in Cube examples through ST-Link , after that J-Link is not able to detect the STM32L476 controller ...

Nucleo L476RG, ADC + DMA, Half vs Complete (HAL)

Posted on September 29, 2015 at 11:29 Hallo, I'm trying to modify an example which uses ADC + DMA, which uses the ST-provided HAL, to my needs. I want to use a buffer and be notified when each half is completed, so I can transfer the ...