Skip to main content
torsten2
Associate III
May 1, 2015
Question

unable to debug using gdb and openocd

  • May 1, 2015
  • 1 reply
  • 731 views
Posted on May 01, 2015 at 11:23

Hello,

I�m quit new to STs micro controllers and openocd. I want to use the STM32L152RE on a Nucleo board. I�ve installed the head version of openocd to get support for this board. I start openocd with following parameters:

  openocd -f board/st_nucleo_l1.cfg

My .gdbinit file looks like this:

  target remote localhost:3333  

  monitor reset

  symbol /Users/todi/ebtks/build/source/ebtks.elf

When starting gdb, it looks like that every time the PC of the CPU is at 0x08000242:

  > arm-none-eabi-gdb

  �

  0x08000242 in ?? ()

  Unable to match requested speed 300 kHz, using 240 kHz

  Unable to match requested speed 300 kHz, using 240 kHz

  adapter speed: 240 kHz

  Breakpoint 1 at 0x800019c: file /Users/todi/ebtks/source/main.cpp, line 26.

According to the elf-file this is within the Reset_Handler:

  0800023c <FillZerobss>:

   800023c: 2300       movs r3, &sharp0

   800023e: f842 3b04  str.w r3, [r2], &sharp4

  08000242 <LoopFillZerobss>:

   8000242: 4b09       ldr r3, [pc, &sharp36] ; (8000268 <LoopFillZerobss+0x26>)

   8000244: 429a       cmp r2, r3

   8000246: f4ff aff9  bcc.w 800023c <FillZerobss>

   800024a: f7ff ffb3  bl 80001b4 <SystemInit>

when ever I try to debug the CPU I do not get to main() but end up with a PC of 0x08000242

  (gdb) monitor reset

  Unable to match requested speed 300 kHz, using 240 kHz

  Unable to match requested speed 300 kHz, using 240 kHz

  adapter speed: 240 kHz

  (gdb) s

  Single stepping until exit from function LoopFillZerobss,

  which has no line number information.

  Note: automatically using hardware breakpoints for read-only addresses.

  WARNING! The target is already running. All changes GDB did to registers will be discarded! Waiting for target to halt.

  ^C

  Program received signal SIGINT, Interrupt.

  0x08000242 in LoopFillZerobss ()

Is the warning a hint that resetting the CPU isn�t working as expected? Are there any addition setting I would have to set with openocd or gdb?

thanks in advance for any help or pointers,

Torsten 

#openocd-gdb-stm32l1
This topic has been closed for replies.

1 reply

torsten2
torsten2Author
Associate III
May 5, 2015
Posted on May 05, 2015 at 17:46

I’ve fixed the problem with a tipp from the openocd mailing list. There is a different method to connect the gdb to the openocd server:

target extended-remote localhost:3333