STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Microcontroller Informational Survey

Posted on October 13, 2015 at 21:54Hello everybody! I am a senior working towards my B.S. in Electrical Engineering and recently started my senior design project. I am one member of a team who is working on developing a program to better expose peop...

USART receive string STM32f429

Posted on October 15, 2015 at 14:06 Hi! I have to receive string from USART and them interpret it and make other function(s) depends of string. I saw Clive's example but could someone tell me how can I interpret string ? Please help me :( ...

mgieroba9 by Associate II
  • 1667 Views
  • 3 replies
  • 0 kudos

problem with 7 segment on stm32

Posted on October 16, 2015 at 09:36i am workin on diplaying no''s on 7 segment via stm32f072b the problem is that the o/p is not appearing on the 7 segment ive connected pins of 7 seg to gpioA and gpioC via a 3.3k resistor the follwing is the code#i...

DMA usages between memory to peripheral

Posted on October 16, 2015 at 07:51Hello.I'm trying to use DMA for graphic LCD control on F429(STM32Cube_FW_F4_V1.8.0).LCD spec is 160x128 and color is 16bit(RGB565) and bus type is 8bit parallel.So I'm using FMC to access LCD and now it's working w...

louiey by Associate II
  • 916 Views
  • 0 replies
  • 0 kudos

I2C Hang problem(HAL Driver)

Posted on October 16, 2015 at 07:22Hi, I'm using STM32F407VE as I2c master and STM32F091Cb as I2c slave .In slave i have stop the i2c communication for some certain interval and start again . at that time the communication between the both is not ha...

FLast.19 by Associate
  • 801 Views
  • 0 replies
  • 0 kudos

6MHz HSE from 8MHz creating many problems?

Posted on October 15, 2015 at 11:52 Hi.I'm using 6MHz external crystal for STM32F0 instead of 8MHz.Following standard setup,i have successfully clocked the APB & AHB at 48MHz via PLL with the following modification on the code pasted below: ...

stm32f4 discovery SDIO write block got cry failed

Posted on October 15, 2015 at 16:34I'm porting SDcard code from FatFS_uSD_FreeRTOS for stm32446_eval in STM32Cube to stm32f4-discovery.Reading blocks seems fine, but writing blocks failed.I debugged with GDB. when write it returned crc failed.here i...

sprhawk by Associate II
  • 958 Views
  • 1 replies
  • 0 kudos

How to use the Virtual Com via ST-Link

Posted on October 12, 2015 at 23:51I have an Discovery board. It has the provision to pass the UART of the target through the on-board ST-Link. I have searched the literature on the board and the manuals. I havent been able to find how this works. I...

rbenesh by Associate II
  • 2251 Views
  • 4 replies
  • 0 kudos

Timer to measure PWM signal and redirect to another GPIO

Posted on October 08, 2015 at 21:45I want to create a PWM pass-through program that will read a PWM duty cycle from an RC receiver on a pin (Pulse-width: 1ms-2ms @ 50Hz) and then output that duty cycle on another GPIO Pin at 50Hz. (eventually, the p...

scook116 by Associate II
  • 1216 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.