Problem in Working Multi channel ADC-1 and ADC-3 Parallely
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-06 11:09 PM
Posted on August 07, 2015 at 08:09
Hi,
I am using two Multi channel ADC's (Controller used is STM103RCT6)
. ADC_1(Multi c
hannel as IN4, IN5, IN6) with DMA1 channel-1 and ADC_3(
Multi c
hannel as IN1, IN2, IN3) with DMA2 channel-5, for capturing the ADC Signals , I am facing a problem when both the DMA's are used parallely,. i.e. i am able to read ADC1 value through DMA1 channel-1, but unable to read ADC3 value usingDMA2 channel-5. I am not facing any problem when using either of ADC 1 or ADC 3 standalone.
so i kindly request you to help me with this issue at the earliest .I have attached configuration code in text format. Kindly look in to it ASAP./* ADC1 DMA1 and ADC3 DMA2 Configuration*/void ADC1_DMA1_conf(){ RCC->APB2ENR |= 0x001; // AFIO clk RCC->AHBENR |= 0x01; // Enable DMA1 peripheral clock (DMA1 has Channel 1 to 7) RCC->AHBENR |= 0x02; // Enable DMA2 peripheral clock (DMA2 has Channel 1 to 5) RCC->APB2ENR |= 0x8200; // enabling the ADC1 clk and ADC3 clk RCC->APB2ENR |= 0x0000004; // enabling the GPIOA clk GPIOA->CRL = 0x000000; // (GPIOA->CRH&0XFFFFF00F); // USART1 TX and Rx enable AFIO->MAPR = 0x0; // Mapped as ADC DMA1_Channel1->CPAR = (int)&ADC1->DR; // PERIPHERAL dress DMA1_Channel1->CMAR = (int)&ADC1_value; // memory address DMA1_Channel1->CNDTR = 3; // number of Data to transfer DMA1_Channel1->CCR = (0xFFEF & DMA1_Channel1->CCR) | 0x00; // DMA1_READ_FROM_PERI (Read from peripheral) DMA1_Channel1->CCR = (0xFFDF & DMA1_Channel1->CCR) | 0x20; // DMA1_CIRCULAR_MODE_ENABLED DMA1_Channel1->CCR = (0xFFBF & DMA1_Channel1->CCR) | 0x00; // DMA1_PERIPHERAL_INC_MODE_DISABLED (Peripheral increment mode disabled) DMA1_Channel1->CCR = (0xFF7F & DMA1_Channel1->CCR) | 0x80; // DMA1_MEMORY_INC_MODE_ENABLED DMA1_Channel1->CCR |= 0x100; // PERIPHERAL size (16-bits) DMA1_Channel1->CCR |= 0x2000; // priority (High) DMA1_Channel1->CCR = (0xF3FF & DMA1_Channel1->CCR) | 0x400; //DMA1_MEMORY_SIZE (16BIT) DMA1_Channel1->CCR |= 0x02; // transfer Complete INT ADC1->CR1 = 0x100; // SCAN_MODE_ENABLE ADC1->CR2 |= 0x00001; // ENABLE_START ADC on ADC1->CR2 |= 0x2; // continue conversion ADC1->CR2 |= 0x100; // ADC1_DMA_MODE_ENABLE ADC1->CR2 |= 0xE0000; // start conversion STRT ADC1->CR2 |= 0x00100000; // ADC1_CONV_ON_EXT_EVENT ADC1->CR2 |= 0x400000; // #define ADC1_START_REGU_CONV ADC1->SQR1 = 0x200000; // ADC1_CHANNEL_SEQ_LENGTH ADC1->SQR3 = 0x18A4; // channel in4, in5, in6 NVIC->ISER[0] |= 0x0800; // DMA_CHANNEL1_NVIC_ENABLE ADC1->CR2 |= 0x70000; // Start conversion of regular channels,Start conversion of injected channels,External trigger conversion mode for regular channels DMA1_Channel1->CCR |= 0x01; // channel enable}void ADC3_DMA2_conf(){ DMA2_Channel5->CPAR = (int)&ADC3->DR; // PERIPHERAL dress DMA2_Channel5->CMAR = (int)&ADC3_value; // memory address DMA2_Channel5->CNDTR = 3; // number of Data to transfer DMA2_Channel5->CCR = (0xFFEF & DMA2_Channel5->CCR) | 0x00; // DMA1_READ_FROM_PERI (Read from peripheral) DMA2_Channel5->CCR = (0xFFDF & DMA2_Channel5->CCR) | 0x20; // DMA1_CIRCULAR_MODE_ENABLED DMA2_Channel5->CCR = (0xFFBF & DMA2_Channel5->CCR) | 0x00; // DMA1_PERIPHERAL_INC_MODE_DISABLED (Peripheral increment mode disabled) DMA2_Channel5->CCR = (0xFF7F & DMA2_Channel5->CCR) | 0x80; // DMA1_MEMORY_INC_MODE_ENABLED DMA2_Channel5->CCR |= 0x100; // PERIPHERAL size (16-bits)// DMA2_Channel5->CCR |= 0x2000; // priority (High) ////// DMA2_Channel5->CCR |= 0x0000; // priority (low) DMA2_Channel5->CCR = (0xF3FF & DMA2_Channel5->CCR) | 0x400; //DMA1_MEMORY_SIZE (16BIT) DMA2_Channel5->CCR |= 0x02; // transfer Complete INT ADC3->CR1 = 0x100; // SCAN_MODE_ENABLE ADC3->CR2 |= 0x00001; // ENABLE_START ADC on ADC3->CR2 |= 0x2; // continue conversion ADC3->CR2 |= 0x100; // ADC3_DMA_MODE_ENABLE ADC3->CR2 |= 0xE0000; // start conversion STRT ADC3->CR2 |= 0x00100000; // ADC2_CONV_ON_EXT_EVENT ADC3->CR2 |= 0x400000; // #define ADC2_START_REGU_CONV ADC3->SQR1 = 0x200000; // ADC2_CHANNEL_SEQ_LENGTH ADC3->SQR3 = 0xC41; // channel in1, in2, in3 // ADC3->CR1 = 0x00; // channel 0 is selected /////// NVIC->ISER[1] |= 0x0800; // DMA2_CHANNEL5_NVIC_ENABLE ADC3->CR2 |= 0x70000; // Start conversion of regular channels,Start conversion of injected channels,External trigger conversion mode for regular channels DMA2_Channel5->CCR |= 0x01; // channel enable}Regardssurender A
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-07 10:34 AM
Posted on August 07, 2015 at 19:34
I wouldn't expect many bites on incomplete register level code.
It's probably not related to the DMA configuration.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..