STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

errors while using DSP lib

Posted on January 17, 2016 at 17:09 hi everyone I'm going to apply FFT on a signal captured by ADC but I've some errors I've tried to fix them but I couldn't can someone kindly help me with a solution. It is good to say that the errors are a...

ghfa0098 by Associate
  • 1339 Views
  • 1 replies
  • 0 kudos

flash memory endurance of STM32F030

Posted on January 17, 2016 at 03:08Hi~ I'm under review for EEPROM emulation on STM32F030. but, I found that flash memory endurance is min 1000 cycle(1K). Unfortunately, It is short to use in my project.Do you know why it is shorter than other STM3...

jaeshik by Associate
  • 1283 Views
  • 1 replies
  • 0 kudos

Input Capture module in pulse count example

Posted on January 16, 2016 at 07:49Hello all,In an external pulse count application, is it possible to capture Timer counts at fixed interval using input capture (IC) module while external input (TIM5_CH1) is driving timer time-base (through TI1F_ED...

rumlyen by Associate II
  • 2520 Views
  • 4 replies
  • 0 kudos

CubeMX and STM32L-Discovery

Posted on January 14, 2016 at 20:21Hi. I'am developer from Russia. And, i have a problem. I generate project in CubeMX with Virtual Com Port (USB 2.0) and upload it in my device (STM32L-Discovery board with STM32L152RBT6). When i connect USB cable (...

0690X00000602aoQAA.jpg 0690X00000602atQAA.jpg

Reload STM32L476-Discovery demonstration on Mac

Posted on January 16, 2016 at 08:24Very much a new learner to these chips and the associated tools (but a long time micro-controller and IT developer).Environment:- STM32L476 Discovery kit- AC6's System Workbench (under Windows 10 ia VM under OSX 10...

Defining SPI2 manually on STM32CubeMx ?

Posted on January 17, 2016 at 00:02 Guys, I want to manually define SPI2, I generated SPI1 from STM32CubeMX, but I have done some modification on some files, and I want to initialize SPI2 myself, is it only at spi.c...or I need t...

New-bie question on Low power modes: Sleep/LP Slepp

Posted on January 16, 2016 at 18:52Hi, I am a beginner and experimenting with low power modes. I'm looking for two answers: 1. Is Sleep mode is mandatory to be configured with HSI, or we can also configure it with HSE 8MHz? SPL example and datasheet...

Cannot connect to a Discovery card with ST-link/V1

Posted on January 15, 2016 at 23:27I have a discovery card F100RBT which is working. I see my old SW blinking LEDs. But now I cannot connect to it. It has been difficult before but now it seems impossible. I have tried with Keil IDE and ST-LINK. Res...

LMI2 by Lead
  • 571 Views
  • 1 replies
  • 0 kudos

Confused about GPIOA->CRL

Posted on January 16, 2016 at 14:19hello I am using STM32Nuleo103 and keil compiler.I was configuring GPIOA->CRL register. I found followingGPIOA->CRL = oxooooooo8; //worksGPIOA->CRL |= oxooooooo8; //Not worksI am confused i am just doing ORing with...

SS.Sagar by Associate III
  • 879 Views
  • 1 replies
  • 0 kudos