2015-08-22 12:36 PM
hi folks,
i've a soft spot for the STM32 series after managing to make a USB audio device a couple of years ago, using a lowly STM32F103. so for a new project i am delighted to find that the price has reduced considerably and that USB2 is available on the STM32F072 series, and i am doing a keyboard-scanner, mouse-pad, SPI-driven LCD, Power Manager and Real-Time clock project. so before i commit to the PCB, i've bought a Nucleo-STM32F072RB and i need to test programming it directly over USB, with openocd. i don't want to be using the STM32103, as that will not be on the final product: i need the STM32F072RB, and that will be emulating USB-HID devices. am i right in thinking that i can pretty much just plug in a USB cable directly into PA11 and PA12, make sure BOOT0 is set correctly, power up and... that's it? much appreciated the advice.2015-08-23 5:50 AM
ok so i've just discovered dfu-util:
http://dfu-util.sourceforge.net/ i believe this is more likely to be what i need. the question is: is it really as simple as connecting USB wires up to PA11 and PA12, then pulling BOOT0 to 1 and nBOOT1 to 1? tia.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.