STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2S on STM32F0

Posted on March 01, 2016 at 19:56So I am trying to output an I2S signal from a STM32F0 but although I believe I am initializing the peripheral correctly I am not getting any signal on the pins. I believe I am enabling the appropriate clocks and have...

luke2 by Associate II
  • 1241 Views
  • 1 replies
  • 0 kudos

Position acquisition

Posted on February 29, 2016 at 21:51Hi.Is there some technique (maybe some kind of MEMS) to determine relative position with 1mm precision in 2 m range? For example moving sensor is located on my palm and the reference point is located on my chest o...

baev_al by Associate III
  • 1456 Views
  • 2 replies
  • 0 kudos

Jump to Bootloader in STM32 through User Flash Memory i.e using Boot 0 and Boot 1 Pins in Boot mode from User Flash memory

Posted on November 13, 2014 at 08:13I have a requirement for firmware upgrade. I am planning to use USB DFU class. But command for firmware upgrade will come from PC application in my case . so i need to switch to bootloader which is there in System...

Please confirm PB12 pin location for STM32F469xx

Posted on February 25, 2016 at 03:23Hi:  Can STM guys help to make sure the PB12 location @ LQFP176 of STM32f469xx. On datasheet (DM00219980) Figure 1 (@page 14). pin 85 is mark as  PH8. However  @ Table 10 (@page59) pin 85 is PB12. Which is correct...

Bug: HAL_GPIO_Init -> GPIO_MODE_AF and EXTI_MODE

Posted on July 28, 2015 at 13:52Combination of GPIO_MODE_AF and EXTI_MODE is non-working.In my case that was NSS pin in SPI Slave Mode.HAL code (stm32fxxx_hal_gpio):      /*--------------------- GPIO Mode Configuration ------------------------*/    ...

STM32L15x: UART Configuration and use problem

Posted on May 14, 2012 at 23:54hi everybody, i have to cinfigure an uart interface of my stm32l152 on STM32l-discovery or STM32-sk evaluation board. I have used to configure the uart peripheral interface the example in the stm32 library called Hyper...

STM32F407 reading from SPI2 only get 0xff

Posted on February 29, 2016 at 10:39Dear STM32 users I am new to STM32 but have experience in many other architectures. I got into everything up and running pretty quick (blinking LED, sending UART ... ). But now I'm stuck with no clue what so ever....

stephan2 by Associate II
  • 1878 Views
  • 3 replies
  • 0 kudos

FSMC - Disable ''burst'' writes

Posted on February 26, 2016 at 02:43 I'm using the FSMC in the STM32L4, but can't figure out how to disable ''burst'' writes. By this, I mean that multiple writes happen within a single CS. When I do multiple writes in a row to external ...

0690X00000605MQQAY.png
dpryan by Associate II
  • 1824 Views
  • 4 replies
  • 0 kudos