User Activity

Posted on October 08, 2015 at 21:45I want to create a PWM pass-through program that will read a PWM duty cycle from an RC receiver on a pin (Pulse-width: 1ms-2ms @ 50Hz) and then output that duty cycle on another GPIO Pin at 50Hz. (eventually, the p...
Posted on October 02, 2015 at 04:36I am experiencing a surprising amount of difficulty trying to set up an STM32 VL Discovery board (STMF100RB) with an IDE (IAR EWARM). I have downloaded the STM_STD_Peripherals.zip. and can open examples from it's f...