STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

512kB chip won't flash, but 2MB will (f429)

Posted on March 04, 2016 at 06:47I'm developing an application using the stm32f429 and have completed the firmware. The total size is only ~300kB so I'm trying to downgrade to the 'VE' version with only 512kb as it's substantially cheaper.On my prot...

STM32F0 Hard Fault Error

Posted on March 02, 2016 at 16:40Hi all,The issue that I am having is that I having is last night I was programming and found that my code suddenly stopped functioning completely. After running in debug mode I found that the code immediately enters ...

eric5709 by Associate II
  • 3349 Views
  • 6 replies
  • 0 kudos

Cannot flash STM32F103 if PLL enabled

Posted on February 26, 2016 at 02:55I'm trying to deal with the setting clocking of STM32F103 MCU without the use of third-party libraries.I wrote several functions for this: http://pastebin.com/kLQS9UmwIf I setup clocking by stm32_rccUseHSE, then e...

kiv by Associate II
  • 2138 Views
  • 4 replies
  • 0 kudos

External oscillator use in STM32F103xxx

Posted on March 04, 2016 at 18:00Can I use an external oscillator module to drive a clock directly into the 'oscillator in' pin?ST documentation only shows crystal with load capacitors. #stm32 #oscillator #-

cgordon by Associate
  • 1131 Views
  • 1 replies
  • 0 kudos

Using ULPI interface to have MCU-to-MCU communication

Posted on March 04, 2016 at 17:18Hi,Anyone knows if it's possible use the ULPI interface for MCU-to-MCU communication??I need to have a high throughput bus communication. Even SPI is not fast enough.I am using the STM32F427.Regards :) #ulpi-stm32...

ababo by Associate II
  • 1126 Views
  • 1 replies
  • 0 kudos

Programming STM32F746 to use TCM interface?

Posted on March 04, 2016 at 15:32I built a test program using STM32CubeMX to test the STM32F746 in TCM flash interface mode (selected from the dialog box brought up by using the Cortex M7 button on the configuration tab).  I imported the project int...

kevin2399 by Associate III
  • 1037 Views
  • 1 replies
  • 0 kudos

STM32CubeMX SDIO F4

Posted on June 03, 2014 at 18:01Hi, I've been trying to get SDIO working on the STM32F4 Discovery board. I've wired up the SD card and created a basic project using CubeMX. The MX_SDIO_SD_Init() function completes successfully but I cannot get the H...

joe by Associate III
  • 5369 Views
  • 9 replies
  • 1 kudos

Resolved! stm3f373 clock and flash latency setting

Posted on March 04, 2016 at 09:19 I worked with stm32f373. To reduce power consumption I change the Hclk to 24Mhz and 48Mhz System clock. (use AHB prescaler to /2) But I confused by flash setting. reference manual said that the latency is 000: Ze...

gazam by Associate
  • 1456 Views
  • 1 replies
  • 0 kudos

STM32F746 discovery - 3D model

Posted on October 30, 2015 at 21:57I can't seam to find a 3D model for the new stm32f746 discovery board. I found the production files for altium designer in schematic pack but *.pcbdoc file is missing so I can not create it myself. Could you please...

dorijan by Associate II
  • 3295 Views
  • 4 replies
  • 0 kudos