STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX for Nucleo-L476-RG base project

Posted on March 15, 2016 at 14:58Dear All.I�ve recently installed STM32Cube MX 4.13.0 on both Ubuntu 14 and Windows 10, with the purpose of generating base code for my Nucleo-L476-RG equipped with MEMS sensors daughterboards.I use SW4STM32 fully upd...

Debugger starts up at wrong address.. sometimes..

Posted on March 22, 2016 at 17:39Hi All, I just started working on a STM32L151. I've setup the debugger to break at first instruction (not main), but when I start debugging the program counter stops at 0x1ff00b84 which isn't even a part of the flash...

texton1 by Associate II
  • 2039 Views
  • 2 replies
  • 0 kudos

STM32CubeMX projects are not work in TrueStudio

Posted on January 19, 2016 at 13:12HiI just made a STM32FCubeMX projects for TrueStudio.But, always compile error.The error message is C:\Users\sohae\Desktop\save\STM32F411BASE\TrueSTUDIO\STM32F411BASE Configuration\Debug/..\..\..\Drivers\CMSIS\Devi...

Auto baud rate detection for UART

Posted on March 16, 2016 at 23:40Hi.I would like to implement auto baud rate detection for UART in STM32F303 uC. There are 4 different detection modes. I understand how each of them works (what is being measured), but don't know, if any of that mode...

matic by Associate III
  • 857 Views
  • 1 replies
  • 0 kudos

FMC

Posted on March 22, 2016 at 13:48

arunease by Associate II
  • 672 Views
  • 1 replies
  • 0 kudos

CDC_Transmit_FS () with you stm32cube (LAST VERSION)

Posted on March 22, 2016 at 16:48Are you kidding? What sense has this function made in this way ?uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len){  uint8_t result = USBD_OK;  /* USER CODE BEGIN 7 */   USBD_CDC_SetTxBuffer(hUsbDevice_0, Buf, Len);...

Marco1 by Associate II
  • 584 Views
  • 0 replies
  • 0 kudos

STM32L15xyE marking layout

Posted on March 22, 2016 at 09:55In STM32L151xE/STM32L152xE datasheet  DocID025433 Rev 8 February 2016, the description of marking of packages (all 5 of them) is titled ''Marking of engineering samples''. This appears to imply that this marking desc...

Interrupt Handler

Posted on March 22, 2016 at 12:46Hi, I have two interrupt with different pre-emption priority.When the higher priority interrupt handler is executed, I would like to ''kill'' the lower priority interrupt handler, if it was running.is it possible?Tha...

sirpak by Associate II
  • 1037 Views
  • 3 replies
  • 0 kudos

timer problem at low period value

Posted on March 21, 2016 at 15:46MCU: STM32F100C6T6 ; clocks: 12MHz externalsysclk=hclk=pclk1=pclk2=12MHzI have configured TIM16 as follow TIM_TimeBaseStructure3.TIM_Period = 5;// TIM_TimeBaseStructure3.TIM_Prescaler = 12-1;// TIM_TimeBaseStructure3...

ionutF by Associate III
  • 851 Views
  • 3 replies
  • 0 kudos