STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trigger the OnePulseMode by software

Posted on April 04, 2016 at 13:37Hello,I want to use the OnePulseMode timer on software demand. On the documentation and even in the HAL the triggering by software is not mentioned only by an external signal is mentioned. I did some testing and by p...

Flash timeout reset target and try again

Posted on April 02, 2016 at 13:51hello, i am using stm32f407. I was working on PWM using timer4 .Accidently i connected VDD pin to 10V. Now my stm is not downloading program and previously downloaded program is also not working . Every time I press ...

2013ee139 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos

STM32F4 DMA Interrupt big latency :(

Posted on April 04, 2016 at 01:43 Hi everybody i work on a project and in my project dma sync by timer1 and timer1 as config for pwm and dma trigger on update event. i have a big problem. my total transient is cost and after finish d...

eittinfo by Associate II
  • 2100 Views
  • 2 replies
  • 0 kudos

STM32F427x.svd

Posted on April 02, 2016 at 16:04This SVD has no entry for the DMA2D peripheral. All the other references I can find indicate that the 427 has the same DMA2D as the 429, is that so?

HAL IRQ Handlers busy waiting

Posted on April 04, 2016 at 11:47Hi @all,I'm using HAL library V1.4 in my current project. While checking error handling functions, I came across some problems with interrupt handling in combination with FreeRTOS (https://sourceforge.net/p/freertos/...

osxMotionFX libs and FreeRTOS

Posted on April 04, 2016 at 11:28Dear All,My colleagues and me are developing in very short time a new product with STM32 and STM MEMS.The hardware is on the go, and we are using Nucleo-L476-RG with X-NUCLEO-IKS01A1 and STEVAL-MKI160V1 for software ...

about timing using F446RE

Posted on April 03, 2016 at 04:39Hi all,   I got a board NUCLEO F446RE. I am using mbed for coding and I saw there are delay function precise up to microsecond. I need to create a series of TTL pulses with period in few microseconds to couple hundre...

llwaeva by Associate II
  • 3068 Views
  • 6 replies
  • 0 kudos

SPI clock is set different for different audio frequency

Posted on April 03, 2016 at 05:04To MCD Application Team and any professional, I read through the source code of  \STM32Cube_FW_F4_V1.10.0\Drivers\BSP\STM32F411E-Discovery\stm32f411e_discovery_audio.c as well as any stm32f4xx_audio.c file.I notice t...

simk0024 by Associate II
  • 1146 Views
  • 1 replies
  • 0 kudos

Problem while enabling I2C & FSMC in STM32F103ZE

Posted on June 29, 2015 at 12:06Hi,I am using STM32F103ZE microcontroller. In which  communicating with external SRAM with FSMC . It is working fine.1)Now I am trying to communicate with an IC which is connected through I2C1 (PB6 : SCL , PB7 : SDA,)...

grv1103 by Associate
  • 2628 Views
  • 5 replies
  • 0 kudos

STM32F429x.SVD

Posted on March 11, 2016 at 16:03I downloaded this from http://www.arm.com/products/processors/cortex-m/cortex-microcontroller-software-interface-standard.php and found what I think is an issue with FLASH.ACR.LATENCY: it’s described as 3 bits wide, ...