cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103R8T6 SWD problem

thanhnt
Associate
Posted on November 01, 2015 at 08:19

Hello everyone,

I am making PCB with STM32F103R8T6 but I have problem with SWD. I connect PCB with ST Link Mini via SWD 

SWCLK <--> PA14

SWDIO <--> PA13

RST <--> NRST

SWIM <--> PB3

GND <--> VCC

3V3 <--> VDD

In Keil, it can recognize SW Device but I cannot download flash it say Flash Download failed - ''Cortex - M3''

However, if I tried to erase full chip I can download flash but after ''Programming Done''  it shows 

Contents mismatch at: 08000000H  (Flash=FFH  Required=60H) !

......

Contents mismatch at: 08000063H  (Flash=FFH  Required=08H) !

and then''Flash Download failed - ''Cortex - M3''''

In this case, if I unplug power and plug power again PCB work.

Can you give me some advise to solve my problem?

Thank you very much.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on November 10, 2015 at 11:04

Hi trung_thanh.nguy.001,

I think that PB3 is not required for SWD configuration.

You may refer to the schematic of

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00267113.pdf

for example to check the connections of STLink component.

I recommend you also to connect using the STLink Utility and do some operations using its graphical interface.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.