STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX and CubeMX Example programs

Posted on May 08, 2016 at 11:07It is far from intuitive how to re-create the functionality of the CubeMX example or Application example programs using CubeMX. So why are they part of the CubeMX repository environment.  For example, I am currently tr...

USART3 on STM32F4-Discovery

Posted on November 30, 2012 at 16:47 Hi! Just before starting my post, i would like to thanks the people of this very very usefull forum. A lots of topics helps me in my newly design. So, yes, i'm designing a new board, and i'm evalu...

DNA-) by Associate III
  • 5020 Views
  • 10 replies
  • 0 kudos

DMA latency by fast ADC acquisition.

Posted on May 10, 2016 at 14:57Hi there, Im currently running into a problem with a stm32F334C8Tx controller. The following data represent my program configuration. _____________________________________________________ Data: -------- System - Clo...

eg7963 by Associate III
  • 1443 Views
  • 2 replies
  • 0 kudos

STM32F767 in action :-)

Posted on May 10, 2016 at 20:58 Hey! I was working on a new design, using an STM32F745, when I noticed a couple of weeks ago, that Farnell had some of the new 767's available. Since I could use some more program memory and SRAM, I immediately purcha...

SOLVED ..stm32f7-discovery board and VCP usart1

Posted on April 24, 2016 at 19:02hiI try to setup serial trough y´the USART1 on stm32f7-discovery using cubemx to make the project.When using usart6 everything works fine but with usart1 trough vcp i can not get it up and running.in my main.c i have...

hjh by Associate III
  • 1440 Views
  • 7 replies
  • 0 kudos

SAI Audio Clicks and Screen flickers on STM32F7-Eval

Posted on January 07, 2016 at 18:24Hi,I've added SAI audio stream to a touchscreen app currently running on the STM32F7 Evaluation board.The screen has worked fine and I've been using DMA2D (ChromArt) to draw blended images quickly.However, now I've...

AndyJT by Associate III
  • 735 Views
  • 1 replies
  • 0 kudos

STM32F103 CAN transmit error Bit dominant Error

Posted on May 09, 2016 at 09:13Hi, i have problem with the CAN bus on a STM32F103C8 (48 pin). I configed the CAN and after the first transmit the bus went to Error and BusOFF state. The I checked the CAN Error status register and the TEC counter is ...

drakula by Associate
  • 2431 Views
  • 3 replies
  • 0 kudos

I2C and SPI emalution on GPIO pins

Posted on May 10, 2016 at 14:35Hello, I need comunicate with EEPROM, 24, 93 and 95 series EEPROM. My micro is STM32F103, there is no I2C, SPI pin free to use. I will emulate these protocol I2C, SPI and Microwire on GPIO pins, always with the same pi...

vbruno1 by Associate III
  • 1245 Views
  • 1 replies
  • 0 kudos