USART2 (PA2, PA3) in polling mode
Posted on May 12, 2016 at 07:17The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on May 12, 2016 at 07:17The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on May 13, 2016 at 09:10I have STM32L4, and I want build a program run at address like 0x08080000. My env is uVision5, and I set the 1ROM1 address to 0x08080000 in uVision. I use fromelf command to generate the bin file from axf file and load...
Posted on May 02, 2016 at 18:13Hello, I found that hcan->State was set to HAL_CAN_STATE_BUSY_TX_RX in HAL_CAN_Transmit_IT() when transmission has started. But successful transmission was not caught and CAN_Transmit_IT() was not called. After that hc...
Posted on May 12, 2016 at 12:57Hello, I have a problem with bitmap displaying using IMAGE_SetBMP as a widget. I can display using GUI_BMP_Draw but I cannot as a item of parent window. Can you help where is a problem? regards, Piotr
Posted on April 25, 2016 at 14:20Hi , I want to generate signal equal to 2.048MHz for audio codec IC which need to be very precise . Right now I have configured TIM8 CHN3 with per-scaler = 0 and period = 40 and timer peripheral clock is around 84 MH...
Posted on May 13, 2016 at 14:49Hi All,I'm using Emcraft's uCLinux deposit. For host-side USB support on the STM32F7 this uses the dwc2 driver. However when I configure the kernel to have gadget support it fails to build.I've read this post (https://...
Posted on May 13, 2016 at 15:49 Hello, I tried to use the TIM2/3/4/5 Input-Capture with DMA (''TIM_DMA_CC1'') to trigger a DMA-Transfer (this writes to a GPIO-Port for parallel Data-transmission) but it just Work with DMA2, not DMA1. ...
Posted on May 13, 2016 at 15:42Hi,I want to update firmware by using the sd card with my stm32f429 mcu. I will connect the sd card to mcu sdio pins ( 1 bit only) , so i will not use spi port for sd card. I just want to learn whether it is possible t...
Posted on May 12, 2016 at 09:24The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 02, 2016 at 11:57 Hi, I tried to configure my STm32F107 using the ''Cube'' to use the CAN1 and user ledsand I found a bug. This is the initialization code generated by the ''Cube'': void HAL_CAN_MspInit(CAN...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.