2015-12-12 5:38 AM
Hello,
i try to get my program work, but im unable to modify the rtc registers. I know that there is a Write Protection, which you can unable by polling the RTOFF Bit and then set the CNF Bit. It doesnt work. I used the CubeMX Code, than my STM std. Lib and than i try it manually by the Debugger, there were no change in the registers. The seconds of the rtc run correct. Cube MX
RTC_TimeTypeDef sTime;
RTC_DateTypeDef DateToUpdate;
RTC_AlarmTypeDef sAlarm;
/**Initialize RTC and set the Time and Date
*/
hrtc.Instance = RTC;
hrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND;
hrtc.Init.OutPut = RTC_OUTPUTSOURCE_ALARM;
hrtc.DateToUpdate.WeekDay = RTC_WEEKDAY_MONDAY;
hrtc.DateToUpdate.Month = RTC_MONTH_JANUARY;
hrtc.DateToUpdate.Date = 1;
hrtc.DateToUpdate.Year = 0;
HAL_RTC_Init(&hrtc);
sTime.Hours = 0;
sTime.Minutes = 0;
sTime.Seconds = 0;
HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BIN);
HAL_RTC_SetDate(&hrtc, &DateToUpdate, FORMAT_BIN);
/**Enable the Alarm A
*/
sAlarm.AlarmTime.Hours = 1;
sAlarm.AlarmTime.Minutes = 2;
sAlarm.AlarmTime.Seconds = 3;
sAlarm.Alarm = RTC_ALARM_A;
HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, FORMAT_BIN);
My onwn code:
set_alarm
while
((RTC->CRL & RTC_FLAG_RSF) == 0)
// wait for last task
{}
RTC->CRL |= RTC_CRL_CNF;
//enter configuration mode
RTC->ALRH = data>>16;
RTC->ALRL = data;
RTC->CRL &= ~RTC_CRL_CNF;
//exit configuration mode
while
((RTC->CRL & RTC_FLAG_RTOFF) == 0)
// wait for last task
{}
the status after MX_RTC_Init()
CRH 0x02
CHL 0x38
PRLH 0x00
PRLL 0x00
DIVH 0x00
DIVL 0x7A28
CNTH 0x00
CNTL 0x00
ALRH 0x00
ALRL 0x00
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.