STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with set priority in STM32F429ZI.

Posted on May 31, 2016 at 11:02#include < main.h > #define Led_Green GPIO_Pin_13 #define Led_Red GPIO_Pin_14 void LED_Config(void) { GPIO_InitTypeDef GPIO_Init_Var={0}; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); GPIO_Init_Var.GPIO_Pin = G...

UART / USART baud rate

Posted on May 27, 2016 at 14:57Is it possible to use baud rate divisor less than 1? i.e. 1/16 - USART_BRR = 0x01I did not find any information about it in STM32F4 RFM.  #uart-usart-baud

aseris by Associate II
  • 1918 Views
  • 6 replies
  • 0 kudos

zany idea: getting more bits resolution out of the ADC

Posted on May 30, 2016 at 16:28The STM32F7 onboard DAC is only 12 bits.  I only need mono audio input.  Suppose I drive the left ADC input directly and the right from an op amp gain stage of say x16 and then combine the lowest 4 bits of R with left-...

dennis by Associate II
  • 3995 Views
  • 3 replies
  • 0 kudos

HASH_RNG_IRQn vs RNG_IRQn in STM32F20x headers

Posted on May 31, 2016 at 11:19Hello, even the V2.1.1 headers for the F2 family still define HASH_RNG_IRQn for the F20x devices that don't have the crypto feature. The F20x header should use RNG_IRQn. Regards #stm32f20x #headers

EXTI_IRQ with USerButton problem

Posted on October 31, 2015 at 15:42 Hello there! I have designed a custom board, and what I'd like to do is that when I press the UserButton, a LED lights up.Now, my button is connected to PC0 pin on my STM32F429 controller, and the LED i...

STM32F4 Discovery LEDs

Posted on May 25, 2016 at 13:00Good morning,Whenever I connect my board via usb, the COM LED lights up solid blue and the LD2 lights up solid green. Does this indicate an error (I'm asking because I haven't been able to get the board to work for a c...

Flash programming FLASH_CR_PER bit not clearing

Posted on May 26, 2016 at 03:06When I try to program flash, I can erase it OK and at the end of erasing I clear the FLASH_CR_PER bit in the FLASH->CR register.When I come to program a pair of half words, I get no errors (FLASH_SR_WRPERR and FLASH_SR...

How can I program my new Discovery board

Posted on May 30, 2016 at 18:38I just purchased a STM32F429I discovery board.  I need to modify the provided software to produce a custom graphics demo for my client.  I downloaded tools from the Keil link on the ST-site, but the libraries are much ...

news by Associate II
  • 991 Views
  • 1 replies
  • 0 kudos

SPI STM32F091 Sending an Data Array

Posted on May 30, 2016 at 19:56 Hello everyone, I have some serious problems i want to send an array of data with SPI but that doesn't work i used the code from the snippet but i changed it a little bit but it doesn't work also in the cod...

sander by Associate
  • 1070 Views
  • 1 replies
  • 0 kudos