cancel
Showing results for 
Search instead for 
Did you mean: 

Same calculation time in both 36MHz and 64MHz

nimamoaddabi
Associate II
Posted on December 15, 2015 at 14:55

Hi everybody

I am trying to implement some mathmatic calculations in STM32F103.

I use HSI and PLL to provide 64MHz and 36MHz clock, considering Flash Wait State and enabling Prefetch Buffer.

 I expect that the calculation time in 64MHz should be faster that 36MHz. As I checked, in both cases, the calculation time is almost same (e.g. 110 usec).

For your information, I used the Timer counter value (e.g. Timer 1) in debug mode (DBGMCU_TIM1_STOP enabled) to calculate the time required for calculation processes. 

 I use the following method to find the calcuation time:

I inserted one break point exactly before first line of mathematics processes and one break point exactly after them.

When the execution of my code is stopped at first break point I record the Timer 1 counter value (e.g. C1=1000).

Then in second break point, I again record the counter value (e.g. C2=8000).

Then I calculate the time by:

(C2-C1)*(1+Tim1Prescaler)/Tim1ClockFrequency=(7000*(1+0)/64MHz)=109 usec.

Each instruction need some clock cycles to do calculations. Therefore, I expect that if the frequency of Clock is increased, then that instruction will be calculated faster. Am I right?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on December 15, 2015 at 17:11

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Calculation%20time%20is%20same%20in%20both%2036MHz%20and%2064MHz%20clock&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=17]Dupe

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..