Skip to main content
rgrimes
Associate III
December 10, 2015
Question

Can't remove write protection from FLASH pages 0 and 1 on STM32F103!

  • December 10, 2015
  • 2 replies
  • 3117 views
Posted on December 10, 2015 at 22:29

Okay, we have a bootloader that we want to replace programmatically, as it is not practical to get access to the debug ports. I've done this successfully with a STM32F071, but have not been able to get it working on a STM32F So the concept is to use the bootloader to load an app that ''simply'' copies a block of data over the bootloader - hence, the bootloader is replaced. Here is an outline of the approach (the printStatus function reports the FLASH_x result to a terminal for viewing).

// Reset - The Option Bytes are copied for the processor's use

// In Bootloader

// Write protect bootloader in first four pages

FLASH_Unlock();

if (FLASH_GetWriteProtectionOptionByte() == 0xffffffff) {

FLASH_EnableWriteProtection(FLASH_WRProt_Pages0to1 | FLASH_WRProt_Pages2to3);

}

FLASH_Lock();

// Point 1 - At this point, the WP bits in the Option Bytes are set,

// but what the processor uses may vary; bootloader relocates vector table here and jumps to the app

// In App, check for WP active

FLASH_Unlock();

FLASH_ClearFlag( . . . );

WRPR_Value = FLASH_GetWriteProtectionOptionByte();

ProtectedPages = ~(WRPR_Value | BL_FLASH_PAGES); // BL_FLASH_PAGES = 3, meaning pages 0 - 3

protected = ((WRPR_Value | (~BL_FLASH_PAGES)) != 0xFFFFFFFF );

// If WP active, unprotect and reboot to cause the OB loader to run

if (protected) {

FLASH_EraseOptionBytes();

NVIC_SystemReset(); // Reset to load new option bytes

// Point 2. Reset occurs

}

// Point 3. After reset and the bootloader writing to the OB, we get here, because the

// protected variable is now false this time.

// Erase the four pages

int i;

uint32_t page = 0x08000000;

for (i = 0; i < 4; ++4) {

FLASH_ClearFlag( . . . );

printStatus(FLASH_ErasePage(page); // Point 4 - page 0 and 1 fail with WPERR, page 2 and 3 succeed!

page += 0x800;

}

// Copy the data

uint16_t* src = start of image;

uint32_t dest;

for (dest = 0x08000000; dest < 0x08002000; dest += 2) {

printStatus(FLASH_ProgramHalfWord(dest, src++); // Point 5 - of course, this fails for pages 0 and 1

}

So the odd thing is that, while the bootloader turns on WP for pages 0 - 3, and the app turns it off for 0 - 3, after the reset, 0 and 1 remain protected, and 2 and 3 are not!

I know the bootloader indeed turns on WP for pages 0 - 3, as I can verify that with ST-LINK. I know the app turns off WP for pages 2 and 3, as they are erased. I know that if the OB are erased, then all WP should be off! Finally, if I use a version of the bootloader that doesn't turn on WP, then the page erasing and programming work correctly!

So the crux of the problem seems to be that pages 0 and 1 are handled specially, somehow? But I cannot find any references to such unusual behavior.

Help, please!

    This topic has been closed for replies.

    2 replies

    rgrimes
    rgrimesAuthor
    Associate III
    December 15, 2015
    Posted on December 15, 2015 at 14:44

    Nobody has any ideas on this?  It's got us rather stuck right now...

    Tesla DeLorean
    Guru
    December 15, 2015
    Posted on December 15, 2015 at 18:10

    Nobody has any ideas on this? It's got us rather stuck right now...

    Forums are an echo chamber for lost souls... I've got some thoughts on this, but it's been several years since I've mined into the F1 parts at this depth. Protection schemes and methods tend to fall into the area of vague documentation, examples and functionality, often purposefully so. You have to get in the trenches and fight with the issues/behaviour there. The logic here seems broken, and the immediate reset might perhaps be an issue

     WRPR_Value = FLASH_GetWriteProtectionOptionByte();
     ProtectedPages = ~(WRPR_Value | BL_FLASH_PAGES); // BL_FLASH_PAGES = 3, meaning pages 0 - 3
     protected = ((WRPR_Value | (~BL_FLASH_PAGES)) != 0xFFFFFFFF );
     
    // If WP active, unprotect and reboot to cause the OB loader to run
     if (protected) {
     FLASH_EraseOptionBytes();
     NVIC_SystemReset(); // Reset to load new option bytes
     
     // Point 2. Reset occurs
     }

    Instrument and confirm it's doing the option erase, and returns success. Perhaps dwell there, or power cycle.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..