STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The problem with the interface QUAD SPI

Posted on June 07, 2016 at 01:59I have STM32F746BGT6 chip and flash memory W25Q64BV - soldered on its own breadboard.Connecting legQUADSPI_BK1_IO0 - PF8QUADSPI_BK1_IO1 - PF9QUADSPI_BK1_IO2 - PF7QUADSPI_BK1_IO3 - PF6QUADSPI_BK1_NCS - PB6QUADSPI_BK1_C...

Avoid ''SD card transfer complete wait'' in case of DMA

Posted on June 07, 2016 at 08:02Hi,I am working on STM32L4xx MCU. I have connected MicroSD card of 8GB size over SDMMC interface. And I am using DMA for write to the SD card.Now, DMA is used to keep the MCU free during that time of data transfer. Bu...

dhaval by Associate II
  • 2449 Views
  • 4 replies
  • 0 kudos

USB/Startup Problem with the new STM32F429 [V2]

Posted on June 07, 2016 at 11:40Hello,my problem should be simple to solve, but due to it's rather undocumented nature I resort on posting it to this forum. When plugging in the STM32F429 board into a pc, it gets detected as flashdrive with around 2...

Resolved! Please help on the filename problem for microSD card

Posted on June 04, 2016 at 01:37 I developed a board using STM32F411 chip with uSD card.The code is generated by cubemx. only add a little bit code in main(). The hardware is OK. I can correctly write a file to sd card. But the weird thing is th...

0690X00000605ORQAY.png 0690X00000605OWQAY.png 0690X00000605LnQAI.png
rwmao by Senior
  • 4354 Views
  • 3 replies
  • 0 kudos

Timer Output Compare mode change in STM32F4

Posted on May 30, 2016 at 10:31Hi!I'm trying to run a bldc motor with stm32f407 IC. The most common method to do that is six-step mode control. I configured TIM1 in complementary mode. but as you know, timer mode must be changed during each step.For...

STM32F103C8T6 failure mode

Posted on June 06, 2016 at 22:26Can anyone here tell by the location of the 'smoke' holes in this STM32F103C8T6 what caused the failure?  There does not appear to be any other failed components on the board.  The boards 3.3v regulator is still worki...

0690X000006035dQAA.jpg
kci by Associate
  • 1034 Views
  • 0 replies
  • 0 kudos

EVALBOARD STM32L476G USART1 receive problem

Posted on June 01, 2016 at 14:23 Hello, I am working on the STM32L476G board, with my own code (except using: stm32l4xx.h, stm32l476xx.h, system_stm32l4xx.h,startup_stm32l476xx.sand core_cm4.h). Which means that i'm building my own usa...

STM32F405/7 Flash SPI problem

Posted on June 06, 2016 at 07:04 Hi there, I have a problem when I'm sending data to and from external SPI chip (Spansion S25FL032P). The problem is I'm getting a really weird signals when I'm over 2,5 MHz speed (see the attached images). I'm...

0690X00000605OlQAI.png 0690X00000605OqQAI.png 0690X00000605P0QAI.png 0690X00000605MHQAY.png
matej2 by Associate II
  • 2377 Views
  • 3 replies
  • 0 kudos