cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 DISCO(MB997) and LIS3DSH using HAL (Read WHO_AM_I return 254)

contacto
Associate
Posted on January 10, 2016 at 18:38

Hello

I am trying configure STM32F4 DISCO to read LIS3DSH using HAL but I have problems on read WHO_AM_I (0x0F) with default value 0011 1111

I generate the configuration in MX cube:

void MX_SPI1_Init(void)

{

  hspi1.Instance = SPI1;

  hspi1.Init.Mode = SPI_MODE_MASTER;

  hspi1.Init.Direction = SPI_DIRECTION_2LINES;

  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

  hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;//LOW;

  hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;//1EDGE;

  hspi1.Init.NSS = SPI_NSS_SOFT;

  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;//4;

  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

  hspi1.Init.TIMode = SPI_TIMODE_DISABLED;

  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;//7;

  HAL_SPI_Init(&hspi1);

main()

{

      ****

      MX_GPIO_Init();

      MX_SPI1_Init();

      HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET);

__HAL_SPI_ENABLE(&hspi1);

     write_accelerator_register(0x20, 0x17, &hspi1);

     write_accelerator_register(0x24, 0x00, &hspi1);

     uint8_t id;

     id=read_accelerator_register(0x0F, &hspi1);

      ****

}

void write_accelerator_register(uint8_t piRegister, uint8_t piData, SPI_HandleTypeDef* phSPI)

{

// Set SS to low to select the accelerator on the SPI interface.

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);

// Send register index which we want to write.

HAL_SPI_Transmit(phSPI, &piRegister, 1, 100);

HAL_SPI_Transmit(phSPI, &piData,     1, 100);

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET);

}

uint8_t read_accelerator_register(uint8_t piRegister, SPI_HandleTypeDef* phSPI)

{

uint8_t iResult = 0;

// Set SS to low to select the accelerator on the SPI interface.

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);

// Set MSB to indicate a read operation.

piRegister |= 0x80;

HAL_SPI_Transmit(phSPI, &piRegister, 1, 100);

HAL_SPI_Receive(phSPI, &iResult, 1, 100);

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET);

return iResult;

}

Can you help me?

Best regards

(Sorry for the english)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on January 12, 2016 at 14:14

Hipeter.john,

For reading a data from the accelerometer, you can use the function:

void ACCELERO_IO_Read(uint8_t *pBuffer, uint8_t ReadAddr, uint16_t NumByteToRead)

It is implemented underSTM32Cube_FW_F4_V1.0\Drivers\BSP\STM32F4-Discovery\stm32f4_discovery.c and it usesSPIx_WriteRead() function which call the functionHAL_SPI_TransmitReceive(). So, as another alternative maybe it will be more efficient if you callHAL_SPI_TransmitReceive() instead ofboth functions HAL_SPI_Transmit() andHAL_SPI_Receive(). -Shahrzad-