STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32L4] Bit banding

Posted on June 15, 2016 at 10:27Hi,I want to use the Bit Banding region of STM32L4 but I do not know how to modify the linker script for the same.I tried to follow the https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?Roo...

sunny by Associate II
  • 3825 Views
  • 11 replies
  • 0 kudos

STM32f429I crashes when activating TIM8

Posted on April 20, 2016 at 17:53Hi, I am using a STM32F429I discovery board and I would like to use the TIM8 with external clock source to trigger ADC conversions. Unfortunately, when I activate and configure TIM8 in STM32CubeMX my application cras...

smrtkai by Senior
  • 2965 Views
  • 11 replies
  • 0 kudos

STM32F767ZI Nucle-144: Higher frequency than 180Mhz.

Posted on June 19, 2016 at 17:16Hi everyone, I am configuring my system_stm32f7xx.c file and I noticed while looking through the reference manual that the max PLL frequency is only 180Mhz. I am looking to get 192Mhz. Does anyone know how to get more...

Configuring SDADC for Repeat Triggering with DMA

Posted on June 22, 2016 at 06:36I need SDADC1 to do a scanned injected DMA conversion of fifty samples total each time there is a TRGO output from TIM4. I have confirmed by measurement using HAL_GetTick() that TIM4 is cycling at the desired rate of ...

spflanze by Associate II
  • 1013 Views
  • 0 replies
  • 0 kudos

ADC and sampling option

Posted on June 22, 2016 at 06:27I want some advice on an programming issue.Using: STM32F107I am running an 10kHz interrupt from PWM channel.Interrupt lasts about 40usec and being contisiously.I need to measure 4 sensors.3 of them are LTS-6NP which g...

SProg by Associate III
  • 667 Views
  • 0 replies
  • 0 kudos

Call to Systick_config causes program to hang

Posted on June 19, 2016 at 22:14 Once I comment out the call to systick it all works as expected, any idea why? I have an Stm32f103c8t6 64kb but Keil thinks its 128kb I changed it to 64 in the debugger settings but aside from that I'm no...

ea6987 by Associate II
  • 2376 Views
  • 6 replies
  • 0 kudos

STM32F0 ADC->DMA touble

Posted on March 26, 2014 at 16:54I have looked over the following code many times. Not sure what the problem is. Any incite? The raw_dma_adc[] array has no values in it during debug. The code is for a STM32F051K6U6. End goal is to have 5 channels r...

USB CDC error recovery

Posted on June 21, 2016 at 01:09I am trying to use USB CDC on STM32F205 from cubemx v4.15.1 with STM32F2 firmware package 1.3.1, all the latest.  Have got almost everything working with the only problem occurring if the host (either Windows or Linux...

gusg by Associate
  • 1267 Views
  • 2 replies
  • 0 kudos

What happened with my STM32

Posted on June 20, 2016 at 16:08[Stm32F103] I can programm flash with ST-LINK utility, but program does not start. Also Keil can't run debug. Keil can programm flash, but stm does nothing. Internet search returned no results.