cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to write the binaries in to stm32f4 using st-link v2 programmer

Kris1
Associate II
Posted on January 19, 2016 at 06:36

Unable to write the binaries in to stm32f4 mcu using st-link v2 programmer. I am using STM32F407VET MCU. When I programming the binaries into it, it shows fwrite fails.

How to unlock the flash of the STM32F4XX using software programming/ Hardware settings.

The following error is occurring:

sudo ./st-flash write main.bin 0x08000000

2016-01-19T11:01:37 INFO src/stlink-usb.c: -- exit_dfu_mode

2016-01-19T11:01:37 INFO src/stlink-common.c: Loading device parameters....

2016-01-19T11:01:37 INFO src/stlink-common.c: Device connected is: F4 device, id 0x10016413

2016-01-19T11:01:37 INFO src/stlink-common.c: SRAM size: 0x30000 bytes (192 KiB), Flash: 0x800000 bytes (8192 KiB) in pages of 16384 bytes

2016-01-19T11:01:37 INFO src/stlink-common.c: Attempting to write 50040 (0xc378) bytes to stm32 address: 134217728 (0x8000000)

EraseFlash - Sector:0x0 Size:0x4000

Flash page at addr: 0x08000000 erasedEraseFlash - Sector:0x1 Size:0x4000

Flash page at addr: 0x08004000 erasedEraseFlash - Sector:0x2 Size:0x4000

Flash page at addr: 0x08008000 erasedEraseFlash - Sector:0x3 Size:0x4000

Flash page at addr: 0x0800c000 erased

2016-01-19T11:01:37 INFO src/stlink-common.c: Finished erasing 4 pages of 16384 (0x4000) bytes

2016-01-19T11:01:37 INFO src/stlink-common.c: Starting Flash write for F2/F4/L4

2016-01-19T11:01:37 INFO src/stlink-common.c: Successfully loaded flash loader in sram

enabling 32-bit flash writes

size: 32768

size: 17272

2016-01-19T11:01:37 INFO src/stlink-common.c: Starting verification of write complete

2016-01-19T11:01:37 ERROR src/stlink-common.c: Verification of flash failed at offset: 0

stlink_fwrite_flash() == -1

thank you in advance.

 

#stm32f407
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on January 19, 2016 at 19:01

Understand that this is a third-party tool, you should probably check with the community/coders around it, although the developer probably doesn't want to personally trouble shoot everyone's problems.

Suggest you use the ST-LINK Utilities and confirm behaviour there, and make sure the firmware is up to date and supported by the tool you are using.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Kris1
Associate II
Posted on January 21, 2016 at 12:53

Thank you, clive.   I used the ST-Utility Programming software, with using it, the problem solved.