STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C slave interrupt issues

Posted on September 02, 2015 at 15:32  The original post was too long to process during our migration. Please click on the attachment to read the original post.

Going to STOP while waiting for UART TX DMA to complete

Posted on July 04, 2016 at 04:06Dear forum, I am trying to transfer a block of bytes from RAM to UART2 using DMA on STM32F042.  I found the HAL function HAL_UART_Transmit_DMA, so I want to go to stop right after that, like this:    int_disable();   ...

hmc by Associate III
  • 1400 Views
  • 2 replies
  • 0 kudos

STM32F746G-DISCO QSPI External Connect

Posted on July 04, 2016 at 15:51I want to connect the interface QSPI external chip, but I can not find a way to override some of the tire contacts the outer connector.Override contacts worked for legs IO0, IO1, IO2, IO3 but I can not override to NSS...

Reset read protection in STM32F205

Posted on November 01, 2012 at 22:15I turned on a test board this morning and could not program or read the flash area (0x0000 0000 to 0x1FFF FFFF).  Looking at the option bytes in FLASH_OPTCR register I see the RDp field set to FF, level 1 protecti...

Reading EEPROM using I2C with HAL library

Posted on July 04, 2016 at 09:30 Hi, I am trying to read the content of an EEPROM,24AA02E48T, using HAL I2C library. There is an example for this task which has been done in SPL instead of HAL and can be found athttps://github.com/Catethys...