STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Clock held low by STM32? STM32 is slave.

Posted on July 11, 2016 at 20:28I've programmed several I2C applications, but never as the slave.Using an STM32F031 Nucleo-32 board, connected to a Linux system with other I2C devices.I would post code examples, but at this point the only code that ...

mattreed9 by Associate III
  • 2293 Views
  • 1 replies
  • 1 kudos

STM32CubeMX - problem after F1 FW package actualisation

Posted on July 10, 2016 at 21:43Hello,I've got a problem with connection error to the target in ST-Link Utility in every program generated by CubeMX with newest FW package for STM32 F1 family (1.4.0). After download program to uC there is error and ...

samat0513 by Associate II
  • 2274 Views
  • 4 replies
  • 0 kudos

Mentor Pads footprint for BGA216/STM32F746?

Posted on July 09, 2016 at 16:21Is the footprint available somewhere. Free? Does the Pads Cad footprint tool create that correctly, if I really need to use it. Or is it possible to import/export the footprint from Eagle. I don't have Eagle Cad, and ...

LMI2 by Lead
  • 1349 Views
  • 2 replies
  • 0 kudos

How to select an old firmware package in projet settings

Posted on July 09, 2016 at 09:31CubeMX V4.15.1I would like to create a new project using an old firmware package for my STM32F4 (1.11.0 or older for instance). I can't find a way to select the version of the package in the project settings.Regards,P...

pdu-fr by Associate II
  • 2832 Views
  • 3 replies
  • 0 kudos

CubeMX grays out STM32F042F6Px USB

Posted on July 08, 2016 at 01:40Version 4.13.0 STM32Cube V1.0 <-- don't know what this is about. In the datasheet for STM32F042x4, STM32F042x6 (ST DocID025832 Rev 4), USB 2.0 full-speed is included.  I have not yet found any provisos for USB 2.0 FS ...

hmc by Associate III
  • 1477 Views
  • 2 replies
  • 0 kudos

Phase Detector/comparator

Posted on July 11, 2016 at 16:08Hi,I want to write a phase comparator on my nucleo-f334.As far as I know, it works like this: two signals are sent in the phase detector. When one of them cross the zero line, a timer/counter is started, and it stops ...

antoine by Associate II
  • 1088 Views
  • 0 replies
  • 0 kudos

STM32F0Discovery External Interrupt Configuration

Posted on July 11, 2016 at 09:15Hi, I've been trying to get going with this dev. board, but I ran into problems with the external interrupt. No matter what I choose in     SYSCFG->EXTICR[0], the PA0 interrupt is always the selected one. Can anyone o...

lab by Associate II
  • 2817 Views
  • 5 replies
  • 1 kudos