STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM1 and TIM2 config for dual ADC

Posted on July 27, 2016 at 15:06 Hi, I have a code, kindly provided by clive1, to use two ADC in dual mode on STM32F334, and it works well. I can modify some parameters, but something (the ADC itself, the DMA to fill the memory array, or ...

antoine by Associate II
  • 2995 Views
  • 8 replies
  • 0 kudos

STM32F103VBT6 debugging problem

Posted on August 03, 2016 at 11:45 Hello there, Recently I developed a PCB board containing the STM32F103VBT6 MCU. Recently, I was using STM32F4 devices without any problems. For this device however, I am unable to debug my target using Segg...

Stop ADC in Continuous Mode

Posted on August 03, 2016 at 08:31Hello there,I'm looking for a possibility to quickly stop and restart the ADC from continuous run on a STM32F446.I use the ADC1 and ADC2 in dual combined regular simultaneous  + injected simultaneous mode with DMA s...

GNU ARM Eclipse plug-ins

Posted on March 05, 2015 at 07:46Mayla,Could you be so kind to update your permanent post and add a link GNU ARM Eclipse plug-ins project? (http://gnuarmeclipse.livius.net/blog/)It is highly portable (Windows/OS X/Linux) and also provides a large co...

System boot mode hardware considerations

Posted on August 02, 2016 at 18:25(This is a resend--the original didn't seem to get posted). Is it advisable to pull-up pins participating in the system bootloader interfaces (USART1  & 2 for the F3)?  If floating, is it possible for the bootloader...

Not compiling...

Posted on August 02, 2016 at 18:37What version of HAL/etc do you have?  I'm not having any luck compiling it with my kit (Keil uVision 5, set to use the F030R8 processor and the 1.4.0 stm32f0xx_hal.h)...

Setting Up Variable Speed Timer on STM32F4

Posted on August 01, 2016 at 20:55I am working on a project that would benefit from a timer whose speed could be changed in real time within the program. Right now I have a timer set up with Tim_CMD, but the prescaler for that is set when it is init...

epalaima by Associate II
  • 1437 Views
  • 4 replies
  • 0 kudos

ST Motor Control firmware

Posted on August 02, 2016 at 14:00Hi,   I would like to evaluate ST's motor control libraries. I have the motor control workbench, which looks great. I would now like the software libraries - the actual motor control code, PMSM, not BLDC, so I can l...

tau by Associate II
  • 1066 Views
  • 1 replies
  • 0 kudos

Trace function too slow? (Keil)

Posted on August 02, 2016 at 14:43I use two ADCs, working together on two different signals.These two signals have the same frequency and amplitude. They are shifted, Signal 2 has a phase of 90°.The DMA put the converted values in an array. This arr...

0690X00000605QcQAI.png
antoine by Associate II
  • 1644 Views
  • 2 replies
  • 0 kudos