cancel
Showing results for 
Search instead for 
Did you mean: 

Upgrade from USB Host Library 2.0.0 to 2.1.0

jdcowpland
Associate II
Posted on June 24, 2014 at 18:02

Hi guys,

I recently upgraded my USB Host libary in one of my programs from version 2.0.0 to version 2.1.0 and it seems to have broken something. When I try to read a file from my USB Flash drive using FatFs, it crashes. Has anyone had any issues similar to this?

EDIT: When I say it crashes, it enters the f_open command in Fatfs and doesn't return a value. The USBH_MSC_Read10 command just seems to constantly return a USBH_MSC_BUSY and so it never exits a loop within the disk_read command. Further digging has led me to the USBH_MSC_HandleBOTXfer function, where after the first call to the read10 command( in diskio.c) the USBH_MSC_BOTXferParam.BOTState is equal to 0, which means that function never executes anything. I can' t find anywhere in the code where it gets set to 0. Anyone know why/where that might be happening?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
o239955_stm1
Associate II
Posted on February 18, 2016 at 06:19

Are there any solutions for this issue?

I have the same Problem. It seems that the Problems occurs randomly, in most cases the function work without any Problem but sometimes it hangs and doesn't return because of a constant USBH_MSC_BUSY