STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

32F746GDISCOVERY solid model

Posted on August 15, 2016 at 18:34I am designing a daughter board for the 32F746GDISCOVERY. Is a solid model of the assembly (step, iges) available?ThanksGene #32f746gdiscovery-3d-model-solid

Display problem of STemWin with STM32F207IG(mouse cursor)

Posted on June 11, 2014 at 08:57Our team is applying STM32F207IG to 800X480 Touch LCD product. To do this, we have purchased STM3220G-EVAL and succeeded in demonstration.Now we are trying to apply STemWin to our board with SSD1963 Driver. We achieve...

STM32L476VG get max ADC sample rate

Posted on August 10, 2016 at 16:38 Hello everyone I am trying to get the ADC working at max sample rate of 5.33Msps. I tested it with a 500Khz sinewave as input but I get 6 samples every period (2us) which is about 3Msps. I set t...

gnu by Associate II
  • 2338 Views
  • 4 replies
  • 0 kudos

Where to find X-CUBE-AUDIO-F7 lib ?

Posted on August 05, 2016 at 22:53Hello, I didn't found on the ST web site the libraries pointed by https://www.google.fr/url?sa=t&rct=j&q=&esrc=s&source=web&cd=4&cad=rja&uact=8&ved=0ahUKEwjRgs3AkqvOAhXQzRoKHSnEBBcQFgg0MAM&url=http://www.st.com/reso...

jmf1 by Senior
  • 878 Views
  • 1 replies
  • 0 kudos

Which ADC channel?

Posted on August 16, 2016 at 17:06I'm converting a bunch of ADC channels, and the ADC is setup to sequence through them.I'm polling the results.How do I determine which channel was just converted?I can't find any calls into the HAL or any registers ...

mattreed9 by Associate III
  • 2737 Views
  • 2 replies
  • 0 kudos

ST-LINK Utility external NOR-FLASH programming

Posted on August 11, 2016 at 12:18Hello. I have ARM MCU board STM32F407 (Schematic: http://www.keil.com/mcbstm32f200/mcbstm32f200-schematics.pdf ) It is connected to NOR FLASH ( http://www.jameco.com/Jameco/Products/ProdDS/1472780.pdf ) who want to ...

stm32f405 failed erase/programming from sector 4-6

Posted on August 17, 2016 at 14:53Hi, I have a stm32f405 on board connected to stlink v2.  I am using both stm32 stlink utility 3.9 as well as stvp 3.3.8. When I erase/program sectors 0-3, all is fine.  Sometime, I receive failure message on erasing...

benedict by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

STM32F373 Bootloader for USART1

Posted on August 17, 2016 at 12:59Hi,It is possible to start the bootloader directly for USART1 from application ?The problem is that the bootloader reconfigure pins that I need during the bootloader run.AN2606 shows in Figure 12 a procedure BL_USAR...

roy2399 by Associate
  • 975 Views
  • 1 replies
  • 0 kudos

External interrupts question

Posted on August 07, 2016 at 18:23Hi.Currently I use PA15 pin as external interrupt. The ISR routine is common for lines 10 through 15 and it is called EXTI15_10_IRQHandler. Now, I would like to have another signal connected to pin PB12, which has s...

matic by Associate III
  • 988 Views
  • 1 replies
  • 0 kudos